Hi,
Is it possible to wake up CC3200 from LPDS using NWP idle connected if the CC3200 has been put in AP mode? For example, I have a use case as follows: I have a CC3200 (A) which is put into AP mode. I also have another CC3200 (B) that is configured to connect to A. Then I put A into LPDS with NWP idle connected.
Question: would it be possible to wake A up from LPDS by sending some packets using B? I know that it would work if A was put in station mode and was setup to connect to an AP/router. However, it didn't seem work for me if A was put into AP mode and there's no other AP or router involved.
Thanks,
TD.