This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC offset value increasing (not fixed) on CC3200 launchpad

Other Parts Discussed in Thread: CC3200

Hi All,

I am evaluating CC3200 launchpad, Now working on ADC (Pin 58 of CC3200 launchpad). As per my previous experince that offset value should be fixed in any hardware. Here I have modify code( ADC example code from SDK of CC3200) as per below:

1. extract ADC value (12-bits) from 32-bit of total data.

2. convert it into mV range.

3. averaging of acquired 4096 samples.

4. and sending it on Teraterm.

I have got below report in which ADC data is near but offset value is changing.

ADC PIN 58 Testing dt: 31/12/2014
Instruments: TI CC3200 Launchpad, Lenovo Laptop, CCS v6 free liecense, Tektronix make Programmable Power Supply PWS4323
Software Detail: OSPL ADC v1
Teraterm Output: Teraterm Output 31_12_2014.docx
Sr.No. Input Voltage (mV) Measured Voltage (mV)
1 50 mV 69 mV
2 100 mV 128 mV
3 150 mV 188 mV
4 200 mV 247 mV
5 250 mV 309 mV
6 300 mV 370 mV
7 350 mV 431 mV
8 400 mV 492 mV
9 450 mV 554 mV
10 500 mV 615 mV
11 550 mV 676 mV
12 600 mV 737 mV
13 650 mV 798 mV
14 700 mV 859 mV
15 750 mV 921 mV
16 800 mV 982 mV
17 850 mV 1043 mV
18 900 mV 1105 mV
19 950 mV 1167 mV
20 1000 mV 1226 mV
21 1050 mV 1289 mV
22 1100 mV 1350 mV
23 1150 mV 1411 mV
24 1200 mV 1471 mV

Please help/guide me If I am going in wrong direction.

Thanks & regards

Bhavdipsinh Rathod