I am looking at using the CC3200 LaunchXL to replace an existing hard-wired (Tx/Rx/0v) serial link.
The existing serial link operates at 250Kbaud. Is this within the current boards capabilities ??
The existing data link is transmitting non-ASCII characters.
I will initially be using it in unsecured more.
Am I right in assuming the only additional thing I will need to do is connect a terminal to one of the devices and configure as a mDNS server?
If I connect a terminal at a more mundane 115.2kbaud, for the mDNS server setting, will the system automatically detect when using at 250kbaud??
If auto baud rate detection employed is there a risk of initially losing the 1st character(s) - these include the header information used to synchronise the data at the receiving end.
I appreciate any confirmation or otherwise for the above.