Hello,
I am working with CC3200 LaunchXL device.
What are the alternate ways of programming the CC3200 device, other than using UniFlash ??
Also, what are alternate ways of flashing files in the Serial Flash ??
Regards,
Abhishek.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Glenn,
Thank you very much for replying.
Actually the thing is that i have prepared a CC3200 based circuit board for my application, but haven't given the same USB hardware present on the CC3200 LaunchXL launchpad.
Hence i am looking for other ways to program it.
I understood that UniFlash is indeed necessary to program the CC3200.
What i am looking for, is in terms of hardware circuitry.
I will search for the keywords given by you, and get back once i go through them.
Thanks once again for replying.
Regards,
Abhishek.
Hi Abhishek,
Currently the only method of doing the initial programming of the CC3200 is by using Uniflash. You can also use a CC3200 Launchpad to program your board. Just use the center pins of J6 and J7 to make the UART connection (assumes 3.3V logic)
Regards,
Aaron
Hello Aaron,
Thank you for replying.
Can you please elaborate the method so that i can implement correctly.
Regards,
Abhishek.