Hi TI Expert!
I'm testing the Bluetopia stack with WL1835 cape on BeagleBone Black and I having some problems need to support to resolve:
- Why LinuxAUDM only permit I did pair and connect direction from WL1835 to smart device and don't permit do invert direction as user can pair and connect to WL1835 from smart device normally? How to solve it?
- With LinuxAUDM source mode feature, after connected to the external sink device liked Bluetooth speaker, I must play the music file by AUDM command, if after connected audio to external sink speaker and I want to use another program as Aplay(not AUDM command) to play the music and streaming to sink speaker then how to do it?
- If having a music playing already on system then when I did connected source mode to external sink speaker then is it auto switch audio stream to remote speaker?
- Why I cannot play all .wav music file on sd memory by AUDM command to stream audio to external sink speaker while I still can play that files onboard with Aplay program and out music to speaker? It warning several errors: WAV file audio data is not in the PCM format, WAV file audio data is not in the PCM format Frequency: 44100 Channels : 2 ,...
Please advise!
Thanks you very much!
Tri.