I have a
cc3100 boost
and CC31xxEmuBoost
I was able to get control to cc3100
with
- provisioning AP mode
- test cc3100 with sdk visual basic examples
after that i tried to test uniflash procedures
i was able to read the version
I tried to use other menu as
Format
Program
Service Pack Update
but mybe i did something bad.
I don't now why but now my cc3100 doesn't work anymore
for example if i try to get the version
i get this answer
18:51:21] Begin GetVersion operation.
[18:51:21] INFO: > Executing Operation: Connect
[18:51:23] INFO: setting break signal
[18:51:23] INFO: --- please restart the device ---
[18:51:38] ERROR: ---reading ACK signal failed---
[18:51:40] INFO: setting break signal
[18:51:40] INFO: --- please restart the device ---
[18:51:55] ERROR: ---reading ACK signal failed---
[18:51:57] INFO: setting break signal
[18:51:57] INFO: --- please restart the device ---
[18:52:12] ERROR: ---reading ACK signal failed---
[18:52:14] INFO: setting break signal
[18:52:14] INFO: --- please restart the device ---
[18:52:29] ERROR: ---reading ACK signal failed---
[18:52:29] FATAL: --- Can't connect to device !! ---
[18:52:29] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3
[18:52:29] INFO: > Executing Operation: Disconnect
[18:52:29] Operation GetVersion returned.
What can i do?