This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Results for Bluetooth HCI qualification test TP/CFC/BV-02-C

We are in the process of Bluetooth 4.0 qualification using the WL1271L chipet (LSR TiWi-BLE module). The compliance lab has requested additional information on the following test case, which they have indicated is often available from the chipset manufacturer:

 [4.0 HCI] TP/CFC/BV-02-C: Verify that IUT returns the buffer size of the controller when receiving the LE Read Buffer Size command or Read Buffer Size command.

Where IUT is the “implementation under test,” The TiWi-BLE module in our case. Does TI have information on this test case for the WL1271L we could make available to the compliance lab?

Thanks!