Adesto Information is here
http://www.adestotech.com/products/enhanced-serial-flash/
Regards
Ed McKernan
Adesto Sales Manager
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Adesto Information is here
http://www.adestotech.com/products/enhanced-serial-flash/
Regards
Ed McKernan
Adesto Sales Manager
One type of Adesto is supported and listed in the Data sheet here - http://www.ti.com/product/CC3200/datasheet/detailed_description#swas0324627
It is the Adesto (AT25DF081A): 8Mb
Others may be supported but not tested, these may include the Fusion range. The requirement for support is that the serial flash supports the JEDEC specification SFDP (serial flash device parameters).
Glenn.
Ed,
Do you have a serial flash part which can provide 8Mbit of memory AND the wide voltage?
Please share the datasheet..
Regards
Prajay
We would also need the following as per our datasheet
1. Sector eraze size : 4KB
2. Pin-out compatibiilty with existing board. I checked this and found that Adesto part is no following a standard flash pinout. This may be acceptable for some of our customers, but there is no way for us to evaluate it directly.