Hi,
I I want to connect with the Radio tool and Uniflash without using the "TI of EVM (CC3100)".
Please let confirmed or no problem with the following connection.
(Please let me check the minimum connection is required pin)
• CC3100 and CC31XXEMUBOOST ( use Radio Tool )
CC3100 CC31XXEMUBOOST
UART1_TX P1.3
UART1_RX P1.4
UART1_CTS P4.4
UART1_RTS P4.5
nHIB P1.5
・CC3100 and CC31XXEMUBOOST Conection (Use Uniflash)
CC3100 CC31XXEMUBOOST
UART1_TX P1.3
UART1_RX P1.4
UART1_CTS P4.4
UART1_RTS P4.5
Best Regards,
hamada