Hi all,
I can't find on launchpad cc3200 datasheet maximum current draw ratings for +3.3v and +5v pins. Where I can find them?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I can't find on launchpad cc3200 datasheet maximum current draw ratings for +3.3v and +5v pins. Where I can find them?
Hi,
5V pin : It's directly routed from USB supply and depends on the source you are connecting the launch pad. If laptop, typically 500 mA.
3.3v pin : It is derived from on board LDO with 5 v input. Please refer in combination of 5v input and LDO specs + CC3200 peak current combination together. CC3200 Peak current consumption are specified in DS.
Regards,
Geet
That means I can draw 500mA without damage the board? I've asked becouse I can't find LDO specifics on Launchbox Datasheet and CC3200 don't provide any informations about Launchbox.