Dear All,
I want to use MAX485 with CC3200 to establish RS485 communication. I need schematic help. I have gone through the Pins of MAX485 and CC3200 UART1 and understood.
In CC3200,
UART1_TX Pin for trasmit data
UART1_RX for Receiving data
UART1 RTS and CTS for flow control (here need guidance)
In MAX485,
DI for drive input coming from controller
RO for received data going to controller
A and B going to network/ PC (here need guidance)
RE and DE connected to controller (here need guidance)
Please guide me of interfacing of these. shall I need any Pull up or Pull down If yes then on which pins?
Waiting for your answer.
Regards
Bhavdipsinh