Hi All,
We are using WL1271 module and configured as wifi direct, and we have following questions.
Other then the antenna tx power what are the other factors which will affect the wifi range..?
Is it possible to change the bite rate and modulations settings at runtime ?
-log-
Cell 02 - Address: 01:23:45:67:89:10
Channel:1
Frequency:2.412 GHz (Channel 1)
Quality=53/70 Signal level=-57 dBm
Encryption key:on
ESSID:"DIRECT-WIFI"
Bit Rates:6 Mb/s; 9 Mb/s; 12 Mb/s; 18 Mb/s; 24 Mb/s
36 Mb/s; 48 Mb/s; 54 Mb/s
Mode:Master
Extra:tsf=000000000280a0a2
Extra: Last beacon: 4200ms ago
IE: Unknown: 00094449524543542D4653
IE: Unknown: 01088C129824B048606C
IE: Unknown: 030101
IE: Unknown: 2A0104
IE: IEEE 802.11i/WPA2 Version 1
Group Cipher : CCMP
Pairwise Ciphers (1) : CCMP
Authentication Suites (1) : PSK
IE: Unknown: DD2F0050F204104A00011010440001021049000600372A000120101100075065742D696D781054000800010050F2040001
Regards,
Manoj