Hi,
I follow the below link to connect my board and samsung tablet.
iw phy `ls /sys/class/ieee80211/` interface add p2p0 type managed
wpa_supplicant -iwlan0 -Dnl80211 -c/etc/wpa_supplicant.conf -N -ip2p0 -Dnl80211 -c/etc/p2p_supplicant.conf &
wpa_cli -ip2p0
p2p_group_add
wpa_cli -ip2p-p2p0-0
wps_pbc
From the tablet I select the displayed device and it shows connecting. In the terminal I could see the below messages.
p2p-p2p0-0: WPS-PBC-ACTIVE
OK
<3>WPS-PBC-ACTIVE
> P2P-PROV-DISC-PBC-REQ 16:b4:84:0c:45:bc p2p_dev_addr=16:b4:84:0c:45:bc pri_dev_type=10-0050F204-5 name='LCC Lennox Contro (SM-' config_methods=0x188 dev_capab=0x25 group_capab=0x0
<3>WPS-ENROLLEE-SEEN 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4 0-00000000-0 0x2148 4 1 [ ]
<3>WPS-ENROLLEE-SEEN 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4 0-00000000-0 0x2148 4 1 [ ]
<3>WPS-ENROLLEE-SEEN 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4 0-00000000-0 0x2148 4 1 [ ]
<3>WPS-ENROLLEE-SEEN 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4 0-00000000-0 0x2148 4 1 [ ]
<3>WPS-ENROLLEE-SEEN 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4 0-00000000-0 0x2148 4 1 [ ]
<3>WPS-ENROLLEE-SEEN 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4 0-00000000-0 0x2148 4 1 [ ]
> p2p-p2p0-0: CTRL-EVENT-EAP-STARTED 16:b4:84:0c:c5:bc
<3>CTRL-EVENT-EAP-STARTED 16:b4:84:0c:c5:bc
> p2p-p2p0-0: CTRL-EVENT-EAP-PROPOSED-METHOD vendor=0 method=1
<3>CTRL-EVENT-EAP-PROPOSED-METHOD vendor=0 method=1
> p2p-p2p0-0: CTRL-EVENT-EAP-PROPOSED-METHOD vendor=14122 method=254
<3>CTRL-EVENT-EAP-PROPOSED-METHOD vendor=14122 method=254
> p2p-p2p0-0: WPS-REG-SUCCESS 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4
<3>WPS-REG-SUCCESS 16:b4:84:0c:c5:bc 4c3575ed-8f06-5b79-94e4-9463b16560c4
> p2p-p2p0-0: WPS-PBC-DISABLE
<3>WPS-PBC-DISABLE
> p2p-p2p0-0: WPS-SUCCESS
<3>WPS-SUCCESS
> p2p-p2p0-0: CTRL-EVENT-EAP-FAILURE 16:b4:84:0c:c5:bc
<3>CTRL-EVENT-EAP-FAILURE 16:b4:84:0c:c5:bc
> p2p-p2p0-0: AP-STA-CONNECTED 16:b4:84:0c:c5:bc p2p_dev_addr=16:b4:84:0c:45:bc
<3>AP-STA-CONNECTED 16:b4:84:0c:c5:bc p2p_dev_addr=16:b4:84:0c:45:bc
> AP-STA-CONNECTED 16:b4:84:0c:c5:bc p2p_dev_addr=16:b4:84:0c:45:bc
After a while the tablet shows the device with tab here to connect and in the terminal below is displayed.
<3>WPS-ENROLLEE-SEEN 44:91:db:03:31:41 311be49c-9aed-55f8-ba32-7a9f9c5ce056 10-0050F204-5 0x4288 0 0 [A093]
> p2p-p2p0-0: AP-STA-DISCONNECTED 16:b4:84:0c:c5:bc p2p_dev_addr=16:b4:84:0c:45:bc
<3>AP-STA-DISCONNECTED 16:b4:84:0c:c5:bc p2p_dev_addr=16:b4:84:0c:45:bc
> AP-STA-DISCONNECTED 16:b4:84:0c:c5:bc p2p_dev_addr=16:b4:84:0c:45:bc
But if I configure my device as below
p2p_find
p2p_peers
p2p_connect 84:dd:20:66:a8:59 pbc freq=2412
Now a popup is displayed in the samsung tablet asking to connect and on giving connect the connect is successful.
Why is it failing in the autonomous mode?
Regards,
Johncy.