This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 network processor hangs while the host controller works everytime.

Other Parts Discussed in Thread: CC3200, ENERGIA

Hi,

This is Amir.

We are using CC3200 module.

Whenever I use the microcontroller part is works for every time but when i use the network processor it doesnt start everytime.

The module started everytime when we used the microcontroller part but when we used the wifi network processor the device didnt start many a time.

It seemed the power at the power pins was not suffiicinent so connected two 100uF/16V capacitors so now the device connects to the wifi but still issue persists.

The device doesnt start everytime.

Please guide!!!!!