I'm having trouble getting the sensor_profile example to work with my CC3200 launchpad. It doesn't seem to be able to connect to my access point that is using WPA security. I can connect successfully using the 'email' example, and I'm using exactly the same values for SSID_NAME, SECURITY_TYPE (SL_SEC_TYPE_WPA), and SECURITY_KEY for both the 'email' and 'sensor_profile' examples. I have no problems with the 'email' example, but when I run the 'sensor_profile' example it says that it is trying to connect to the correct SSID name, but then times out and tries again, never with any success. Any advice would be appreciated.
Thanks,
Andy