This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uim:poll broke due to event 10(PRI:2/ERR:8)

Hi,

I am trying to get the bluetooth up on wl18xx chip, but I get following error 'uim:poll broke due to event 10(PRI:2/ERR:8)':

# uim &
[1] 182
uim:@ main
uim:install = /sys/devices/platform/kim/install
uim:dev_name = /sys/devices/platform/kim/dev_name
uim:baud_rate = /sys/devices/platform/kim/baud_rate
uim:flow_cntrl = /sys/devices/platform/kim/flow_cntrl
uim:begin polling...
#
#
#
# rfkill  unblock bluetooth
#
# hciconfig hci0
hci0:   Type: BR/EDR  Bus: UART
        BD Address: 00:00:00:00:00:00  ACL MTU: 0:0  SCO MTU: 0:0
        DOWN
        RX bytes:0 acl:0 sco:0 events:0 errors:0
        TX bytes:0 acl:0 sco:0 commands:0 errors:0

# hciconfig hci0  up
uim:poll broke due to event 10(PRI:2/ERR:8)

uim:read 1 from install

uim:@ st_uart_config
uim: signal received, opening /dev/ttyO4
uim:@ set_baud_rate
uim:set_baud_rate() done
uim:Setting speed to 3000000
uim:@ read_command_complete
uim: Command complete started
uim:@ read_hci_event
uim: read_hci_event
uim:Command complete done
uim:Speed changing to 3000000, 1
uim:@ set_custom_baud_rate
uim:Installed N_TI_WL Line displine
uim:begin polling...
#
# hciconfig
hci0:   Type: BR/EDR  Bus: UART
        BD Address: 34:B1:F7:E2:DE:CB  ACL MTU: 1021:6  SCO MTU: 180:4
        UP RUNNING
        RX bytes:348 acl:0 sco:0 events:11 errors:0
        TX bytes:49 acl:0 sco:0 commands:11 errors:0

#

Dmesg output:

[   42.840000] hci0 d6782800
[   42.840000] (stc): st_register(2)
[   42.840000] (stc):  chnl_id list empty :2
[   42.840000] (stk) : st_kim_start
[   42.940000] (stk) :ldisc_install = 1
[   42.990000] (stc): st_tty_open
[   42.990000] (stk) : line discipline installed
[   43.000000] (stk) :TIInit_11.8.32.bts
[   43.000000] PM: Adding info for No Bus:kim
[   43.000000] PM: Removing info for No Bus:kim
[   43.000000] (stk) :change remote baud rate command in firmware
[   43.000000] (stk) :skipping the wait event of change remote baud
[   43.000000] (stc): add_channel_to_table: id 2
[   43.000000] (stc): st_register(3)
[   43.000000] (stc): add_channel_to_table: id 3
[   43.000000] (stc): st_register(4)
[   43.000000] (stc): add_channel_to_table: id 4
[   43.000000] hci0: type 1 len 4hci0: type 1 len 4hci0: type 1 len 4hci0: type 1 len 4hci0: type 1 len 4hci0: type 1 len 4hci0: type 1 len 4hci0: type 6
#

Thanks And Regards,

Mike