Hi,
after having a look at the Service Pack, the following two files are available for OTA:
ota_1.0.0.10.0.ucf.signed.bin
ota_1.0.0.10.0.ucf.ucf
We do not use the TI OTA mechanism and I am now wondering in which folder and with which filenames I should put these files, to update the firmware of the NWP.
I am working under the assumption that either we or Uniflash have already allocated an appropriate size for these files (AFAIK 128 kB, COMMIT mode).
Thanks
Tobias