This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i devolop a androd APP ,send a post request,param is "__SL_P_ULD=LED1_ON" ,IAR open Ti sample project(named out_of_box),then set breakpoint at SimpleLinkHttpServerCallback function,then trigger normal. but then param is not "__SL_P_ULD=LED1_ON"(such as “ABC”..),send a post request ,SimpleLinkHttpServerCallback could not by trigger.what 's wrong ?
static unsigned char POST_token[] = "__SL_P_ULD";
void SimpleLinkHttpServerCallback(SlHttpServerEvent_t *pSlHttpServerEvent,
SlHttpServerResponse_t *pSlHttpServerResponse)
{
switch (pSlHttpServerEvent->Event)
{
case SL_NETAPP_HTTPPOSTTOKENVALUE_EVENT:
{
unsigned char led;
unsigned char *ptr = pSlHttpServerEvent->EventData.httpPostData.token_name.data;//..................breakpoint is here.
//g_ucLEDStatus = 0;
if(memcmp(ptr, POST_token, strlen((const char *)POST_token)) == 0)
{