This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WPA2 Enterprise PEAPv1Mode problem

Other Parts Discussed in Thread: WL1271

Hi

I have tried to connect the WL1271 in WPA2 Enterprise mode with PEAPv1/Mschapv2

WL1271 chipset solution is not able to associate with the AP and it is displaying on the host terminal as "OpenSSL: tls_connection_handshake - Failed to read possible Application Data error:00000000:lib(0):func(0):reason(0)".After this message wpa_supplicant is killing itself.

config file in wpa_supplicant.txt

ctrl_interface=/var/run
ap_scan=2
update_config=0

network={
        ssid="WPA2"
        proto=RSN
        key_mgmt=WPA-EAP
        pairwise=CCMP
        group=CCMP
        auth_alg=OPEN
        eap=PEAP
        identity="janardhan"
        password="jan123"
        ca_cert="/etc/cert/root.pem"
        phase1="peaplabel=1"
        phase2="auth=MSCHAPV2"
        priority=2
}


Regards,

Janardhan