Hi
I am trying to do IOS app. However, the way to make CC3200 board is little complicated as you need to connect the MYSIMPLELINK AP ,type 192.168.1.1 to enter the on board website and enter the ssid name as well as keyword. I want to know if there is anyway to make CC3200 connect to Internet through mobile phone only.
The ideal case is that:
1. mobile phone connect to "MYSIMPLELINK XXX"
2. the phone will show a list of wifi scanned by CC3200 using sl_WlanGetNetworklist
3.choose one of them and type the keyword
4. Once done, disconnect "MYSIMPLELINK xx" and the CC3200 board already connected to internet
Thanks
Heng