Hi, is it possible to add an external WiFi antenna to CC3200MODLAUNCHXL board? The board has RF connectors, but I am not sure how they are used. Can I use those connectors for an external WiFi antenna?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, is it possible to add an external WiFi antenna to CC3200MODLAUNCHXL board? The board has RF connectors, but I am not sure how they are used. Can I use those connectors for an external WiFi antenna?
Thank you.
Hi Raghavendra, thank you for your reply. Section 2.7 states:
2.7 RF Connections
2.7.1 Radiated Testing (AP connection)
By default the board ships with the RF signals routed to the on-board chip antenna. An on-board u.fl
(Murata) connector provides a means to perform the testing in the lab using a compatible cable.
If I understand right the connectors are used for RF testing. I need to use an external antenna to amplify RF signals to get a better RF range. Can I use those connectors to do that. If yes, which one of them I can use?
Thank you.
Hi,
The antenna is not part of the CC3200MOD itself and the user should have the antenna on his board.
The EVM CC3200MODLAUNCHXL has 3 options as mentioned: On board chip antenna, u.fl and muRata connector. The default is the on board chip antenna and this is the option that was taken for the certification.
The other 2 alternatives are provided for users to be able to evaluate with other antenna options and you can use either one. If you use the u.fl you also need to change a resostor on the board to open this path.
Ben