i wrote a program using CCS and it runs on the 3200 launchad (in the CCS using the debug button)
what are the steps needed to be done in order to have my program run on the 3200 mod
1) what do i need to do in the CCS in order to export the program to a file
2)how do i flash it to the 3200 mod using uniflash ?
3) is the flashing through the uart legs? which ones?