Hi everyone!
I'm customizing on Panther Board with android 4.1.2 and I have a issue with wifi module.
Currently, with non-secured network, module wifi works fine.
But, when i try to connect with secured network, the module can't work.
The wifi firmware version is 6.3.9.0.120, i alo try other version, but not successfully.
Any suggestions for my issue.
This is my kernel log:
<5>[ 0.000000] Linux version 2.6.37 (hoavn@hibk-MS-7846) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 Mon May 18 17:03:52 FNT 2015
<4>[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
<4>[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
<4>[ 0.000000] Machine: OMAP3 Beagle Board
<6>[ 0.000000] Reserving 8388608 bytes SDRAM for VRAM
<4>[ 0.000000] Memory policy: ECC disabled, Data cache writeback
<6>[ 0.000000] OMAP3630 ES1.2 (l2cache iva sgx neon isp 192mhz_clk )
<6>[ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000
<7>[ 0.000000] On node 0 totalpages: 129024
<7>[ 0.000000] free_area_init_node: node 0, pgdat c06d2454, node_mem_map c07a1000
<7>[ 0.000000] Normal zone: 1024 pages used for memmap
<7>[ 0.000000] Normal zone: 0 pages reserved
<7>[ 0.000000] Normal zone: 128000 pages, LIFO batch:31
<7>[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
<7>[ 0.000000] pcpu-alloc: [0] 0
<4>[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 128000
<5>[ 0.000000] Kernel command line: init=/init console=ttyO2,115200n8 noinitrd ip=off androidboot.console=ttyO2 rootwait mem=512M omap_vout.vid1_static_vrfb_alloc=y rw ubi.mtd=4,2048 rootfstype=ubifs root=ubi0:rootfs rootdelay=2 vram=8M omapfb.vram=0:8M
<6>[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
<6>[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
<6>[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
<6>[ 0.000000] Memory: 504MB = 504MB total
<5>[ 0.000000] Memory: 503748k/503748k available, 20540k reserved, 0K highmem
<5>[ 0.000000] Virtual kernel memory layout:
<5>[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
<5>[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
<5>[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
<5>[ 0.000000] vmalloc : 0xe0800000 - 0xf8000000 ( 376 MB)
<5>[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
<5>[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
<5>[ 0.000000] .init : 0xc0008000 - 0xc0040000 ( 224 kB)
<5>[ 0.000000] .text : 0xc0040000 - 0xc068a000 (6440 kB)
<5>[ 0.000000] .data : 0xc068a000 - 0xc06d7900 ( 311 kB)
<6>[ 0.000000] NR_IRQS:409
<6>[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/600 MHz
<6>[ 0.000000] Reprogramming SDRC clock to 400000000 Hz
<3>[ 0.000000] dpll3_m2_clk rate change failed: -22
<6>[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
<6>[ 0.000000] Total of 96 interrupts on 1 active controller
<6>[ 0.000000] GPMC revision 5.0
<4>[ 0.000000] Trying to install interrupt handler for IRQ402
<4>[ 0.000000] Trying to install interrupt handler for IRQ403
<4>[ 0.000000] Trying to install interrupt handler for IRQ404
<4>[ 0.000000] Trying to install interrupt handler for IRQ405
<4>[ 0.000000] Trying to install interrupt handler for IRQ406
<4>[ 0.000000] Trying to install interrupt handler for IRQ407
<4>[ 0.000000] Trying to install interrupt handler for IRQ408
<3>[ 0.000000] Trying to install type control for IRQ409
<3>[ 0.000000] Trying to set irq flags for IRQ409
<6>[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
<4>[ 0.000000] Console: colour dummy device 80x30
<6>[ 0.000000] Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)
<6>[ 0.000000] pid_max: default: 32768 minimum: 301
<6>[ 0.000000] Security Framework initialized
<4>[ 0.000000] Mount-cache hash table entries: 512
<6>[ 0.000000] CPU: Testing write buffer coherency: ok
<6>[ 0.000000] regulator: core version 0.5
<6>[ 0.000000] regulator: dummy:
<6>[ 0.000000] NET: Registered protocol family 16
<6>[ 0.000000] OMAP GPIO hardware version 2.5
<6>[ 0.000000] OMAP GPIO hardware version 2.5
<6>[ 0.000000] OMAP GPIO hardware version 2.5
<6>[ 0.000000] OMAP GPIO hardware version 2.5
<6>[ 0.000000] OMAP GPIO hardware version 2.5
<6>[ 0.000000] OMAP GPIO hardware version 2.5
<4>[ 0.000000] Hi253: Da set clock ra
<6>[ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0
<6>[ 0.000000] Found NAND on CS0
<6>[ 0.000000] Registering NAND on CS0
<3>[ 0.000000] Unable to get DVI reset GPIO
<6>[ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported.
<6>[ 0.000000] OMAP DMA hardware revision 5.0
<4>[ 0.027984] bio: create slab <bio-0> at 0
<6>[ 0.029235] regulator: vwl1271: 1800 mV
<5>[ 0.030822] SCSI subsystem initialized
<6>[ 0.033508] usbcore: registered new interface driver usbfs
<6>[ 0.033721] usbcore: registered new interface driver hub
<6>[ 0.033966] usbcore: registered new device driver usb
<6>[ 0.035186] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz
<6>[ 0.048217] twl4030: PIH (irq 7) chaining IRQs 368..375
<6>[ 0.048248] twl4030: power (irq 373) chaining IRQs 376..383
<6>[ 0.048858] twl4030: gpio (irq 368) chaining IRQs 384..401
<6>[ 0.052337] regulator: VUSB1V5: 1500 mV normal standby
<6>[ 0.052947] regulator: VUSB1V8: 1800 mV normal standby
<6>[ 0.053558] regulator: VUSB3V1: 3100 mV normal standby
<6>[ 0.056884] twl4030_usb twl4030_usb: Initialized TWL4030 USB module
<6>[ 0.058349] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby
<6>[ 0.059020] regulator: VDAC: 1800 mV normal standby
<6>[ 0.059661] regulator: VDVI: 1800 mV normal standby
<6>[ 0.060363] regulator: VAUX3: 2800 mV normal
<6>[ 0.061096] regulator: VAUX4: 1800 mV normal standby
<6>[ 0.061309] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
<6>[ 0.070068] omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
<6>[ 0.071929] Advanced Linux Sound Architecture Driver Version 1.0.23.
<6>[ 0.072753] Bluetooth: Core ver 2.15
<6>[ 0.072967] NET: Registered protocol family 31
<6>[ 0.072967] Bluetooth: HCI device and connection manager initialized
<6>[ 0.072998] Bluetooth: HCI socket layer initialized
<6>[ 0.073455] Switching to clocksource 32k_counter
<6>[ 0.100555] musb-hdrc: version 6.0, otg (peripheral+host), debug=0
<6>[ 0.100677] musb-hdrc musb-hdrc.0: dma type: dma-inventra
<7>[ 0.100738] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
<7>[ 0.100769] musb-hdrc: MHDRC RTL version 1.800
<7>[ 0.100799] musb-hdrc: setup fifo_mode 4
<7>[ 0.100799] musb-hdrc: 28/31 max ep, 16384/16384 memory
<6>[ 0.101013] musb-hdrc musb-hdrc.0: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
<6>[ 0.101562] NET: Registered protocol family 2
<6>[ 0.101745] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
<6>[ 0.102203] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
<6>[ 0.102569] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
<6>[ 0.102783] TCP: Hash tables configured (established 16384 bind 16384)
<6>[ 0.102783] TCP reno registered
<6>[ 0.102813] UDP hash table entries: 256 (order: 0, 4096 bytes)
<6>[ 0.102844] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
<6>[ 0.103027] NET: Registered protocol family 1
<6>[ 0.103393] RPC: Registered udp transport module.
<6>[ 0.103393] RPC: Registered tcp transport module.
<6>[ 0.103424] RPC: Registered tcp NFSv4.1 backchannel transport module.
<4>[ 0.103607] NetWinder Floating Point Emulator V0.97 (double precision)
<6>[ 0.105194] omap-iommu omap-iommu.0: isp registered
<6>[ 0.105499] AM37x/DM37x Linux PSP version 04.02.00.07 (OMAP3BEAGLE)
<6>[ 0.263061] ashmem: initialized
<5>[ 0.263549] VFS: Disk quotas dquot_6.5.2
<4>[ 0.263641] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
<6>[ 0.265289] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
<6>[ 0.265960] msgmni has been set to 983
<6>[ 0.267242] io scheduler noop registered
<6>[ 0.267242] io scheduler deadline registered
<6>[ 0.267395] io scheduler cfq registered (default)
<6>[ 0.323791] OMAP DSS rev 2.0
<6>[ 0.323883] OMAP DISPC rev 3.0
<6>[ 0.323913] OMAP VENC rev 2
<6>[ 0.324218] OMAP DSI rev 1.0
<6>[ 0.652832] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
<6>[ 0.654785] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
<6>[ 0.655181] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
<6>[ 0.655548] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
<6>[ 1.354858] console [ttyO2] enabled
<6>[ 1.358978] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
<6>[ 1.378875] brd: module loaded
<6>[ 1.387573] loop: module loaded
<6>[ 1.391235] (stk) :sysfs entries created
<6>[ 1.395416] (stk) : debugfs entries created
<3>[ 1.402313] mtdoops: mtd device (mtddev=name/number) must be supplied
<6>[ 1.409271] omap2-nand driver initializing
<6>[ 1.413970] NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix )
<5>[ 1.420867] Creating 5 MTD partitions on "omap2-nand.0":
<5>[ 1.426452] 0x000000000000-0x000000080000 : "X-Loader"
<5>[ 1.433898] 0x000000080000-0x0000001c0000 : "U-Boot"
<5>[ 1.441223] 0x0000001c0000-0x000000280000 : "U-Boot Env"
<5>[ 1.448516] 0x000000280000-0x000000780000 : "Kernel"
<5>[ 1.457336] 0x000000780000-0x000020000000 : "File System"
<6>[ 1.672454] OneNAND driver initializing
<5>[ 1.677368] UBI: attaching mtd4 to ubi0
<5>[ 1.681365] UBI: physical eraseblock size: 131072 bytes (128 KiB)
<5>[ 1.687988] UBI: logical eraseblock size: 126976 bytes
<5>[ 1.693664] UBI: smallest flash I/O unit: 2048
<5>[ 1.698608] UBI: sub-page size: 512
<5>[ 1.703430] UBI: VID header offset: 2048 (aligned 2048)
<5>[ 1.709747] UBI: data offset: 4096
<5>[ 2.738037] UBI: max. sequence number: 0
<5>[ 2.763824] UBI: volume 0 ("rootfs") re-sized from 3717 to 3992 LEBs
<5>[ 2.771514] UBI: attached mtd4 to ubi0
<5>[ 2.775451] UBI: MTD device name: "File System"
<5>[ 2.781250] UBI: MTD device size: 504 MiB
<5>[ 2.786468] UBI: number of good PEBs: 4036
<5>[ 2.791381] UBI: number of bad PEBs: 0
<5>[ 2.796051] UBI: number of corrupted PEBs: 0
<5>[ 2.800720] UBI: max. allowed volumes: 128
<5>[ 2.805541] UBI: wear-leveling threshold: 4096
<5>[ 2.810485] UBI: number of internal volumes: 1
<5>[ 2.815155] UBI: number of user volumes: 1
<5>[ 2.819824] UBI: available PEBs: 0
<5>[ 2.824493] UBI: total number of reserved PEBs: 4036
<5>[ 2.829681] UBI: number of PEBs reserved for bad PEB handling: 40
<5>[ 2.836090] UBI: max/mean erase counter: 1/0
<5>[ 2.840576] UBI: image sequence number: 855760460
<5>[ 2.845672] UBI: background thread "ubi_bgt0d" started, PID 577
<6>[ 2.870788] usbcore: registered new interface driver asix
<6>[ 2.886169] usbcore: registered new interface driver cdc_ether
<6>[ 2.892486] usbcore: registered new interface driver smsc95xx
<6>[ 2.901794] usbcore: registered new interface driver net1080
<6>[ 2.917419] usbcore: registered new interface driver cdc_subset
<6>[ 2.933044] usbcore: registered new interface driver zaurus
<6>[ 2.948669] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
<4>[ 2.955627] ehci-omap.0 supply hsusb1 not found, using dummy regulator
<6>[ 3.964202] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
<6>[ 4.815826] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
<6>[ 4.831512] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
<6>[ 4.847015] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
<6>[ 4.853149] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
<6>[ 4.860290] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>[ 4.867889] usb usb1: Product: OMAP-EHCI Host Controller
<6>[ 4.873443] usb usb1: Manufacturer: Linux 2.6.37 ehci_hcd
<6>[ 4.879119] usb usb1: SerialNumber: ehci-omap.0
<6>[ 4.925598] hub 1-0:1.0: USB hub found
<6>[ 4.929534] hub 1-0:1.0: 3 ports detected
<6>[ 4.972137] Initializing USB Mass Storage driver...
<6>[ 4.977539] usbcore: registered new interface driver usb-storage
<6>[ 4.983856] USB Mass Storage support registered.
<6>[ 4.988739] android init
<6>[ 4.991455] android_probe pdata: c069a888
<6>[ 5.011108] android_bind
<7>[ 5.013763] android_bind_config
<6>[ 5.026824] android_usb gadget: android_usb ready
<6>[ 5.031738] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
<6>[ 5.042449] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
<6>[ 5.058013] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
<6>[ 5.065155] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>[ 5.072723] usb usb2: Product: MUSB HDRC host driver
<6>[ 5.077941] usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
<6>[ 5.083618] usb usb2: SerialNumber: musb-hdrc.0
<6>[ 5.120971] hub 2-0:1.0: USB hub found
<6>[ 5.124908] hub 2-0:1.0: 1 port detected
<6>[ 5.129089] musb android_usb gadget disconnected.
<6>[ 5.151733] f_adb init
<6>[ 5.154205] android_register_function adb
<6>[ 5.158386] f_mass_storage init
<6>[ 5.161773] fsg_probe pdev: c069a4e0, pdata: c069ab60
<6>[ 5.182983] android_register_function usb_mass_storage
<6>[ 5.188385] adb_bind_config
<6>[ 5.206481] android_usb gadget: Mass Storage Function, version: 2009/09/11
<6>[ 5.213714] android_usb gadget: Number of LUNs=1
<6>[ 5.218566] lun0: LUN: removable file: (no medium)
<6>[ 5.238250] mice: PS/2 mouse device common for all mice
<3>[ 5.253570] gpio-keys gpio-keys: failed to request GPIO 0, error -16
<4>[ 5.260314] gpio-keys: probe of gpio-keys failed with error -16
<6>[ 5.268951] usb 1-2: new high speed USB device using ehci-omap and address 2
<6>[ 5.284759] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input0
<6>[ 5.315948] using rtc device, twl_rtc, for alarms
<6>[ 5.320739] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
<4>[ 5.331451] twl_rtc twl_rtc: Power up reset detected.
<6>[ 5.347259] twl_rtc twl_rtc: Enabling TWL-RTC.
<6>[ 5.355010] i2c /dev entries driver
<6>[ 5.371520] Linux media interface: v0.10
<6>[ 5.386199] Linux video capture interface: v2.00
<4>[ 5.391540] omap3isp supply VDD_CSIPHY1 not found, using dummy regulator
<4>[ 5.398620] omap3isp supply VDD_CSIPHY2 not found, using dummy regulator
<6>[ 5.405822] omap3isp omap3isp: Revision 15.0 found
<6>[ 5.410888] omap-iommu omap-iommu.0: isp: version 1.1
<7>[ 5.416320] omap3isp omap3isp: hist: DMA channel = 0
<6>[ 5.449249] usb 1-2: New USB device found, idVendor=0424, idProduct=9514
<6>[ 5.456268] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0
<6>[ 5.481323] hub 1-2:1.0: USB hub found
<6>[ 5.485473] hub 1-2:1.0: 5 ports detected
<4>[ 5.496154] Hi253: hi253_probe!
<4>[ 5.499481] Hi253: register successful as a media entity
<4>[ 5.511108] Hi253: hi253_s_config
<4>[ 5.514587] Hi253: hi253_dev_init
<7>[ 5.584747] omap3isp omap3isp: isp_set_xclk(): cam_xclka set to 24685714 Hz
<4>[ 5.584747] Hi253: hi253_detect
<4>[ 5.643951] hi253_write_reg: write reg error:reg=3, val=0
<4>[ 5.649597] Hi253: hi253_read_reg
<3>[ 5.659515] hi253_read_reg:write reg error:reg=4
<3>[ 5.664367] hi253 2-0020: chip id mismatch read 0xffff, expecting 0x92
<7>[ 5.683441] omap3isp omap3isp: isp_set_xclk(): cam_xclka set to 0 Hz
<3>[ 5.691162] isp_register_subdev_group: Unable to register subdev hi253
<6>[ 5.706970] usbcore: registered new interface driver uvcvideo
<6>[ 5.712982] USB Video Class driver (v1.0.0)
<6>[ 5.722198] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
<3>[ 5.737976] twl4030_wdt twl4030_wdt: Failed to register misc device
<4>[ 5.744567] twl4030_wdt: probe of twl4030_wdt failed with error -16
<6>[ 5.769256] device-mapper: uevent: version 1.0.3
<6>[ 5.785064] device-mapper: ioctl: 4.18.0-ioctl (2010-06-29) initialised: dm-devel@redhat.com
<6>[ 5.794128] Bluetooth: HCI UART driver ver 2.2
<6>[ 5.798767] Bluetooth: HCI H4 protocol initialized
<6>[ 5.803833] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
<6>[ 5.811035] usb 1-2.1: new high speed USB device using ehci-omap and address 3
<6>[ 5.831420] cpuidle: using governor ladder
<6>[ 5.835723] cpuidle: using governor menu
<4>[ 5.848236] mmci-omap-hs.0 supply vmmc_aux not found, using dummy regulator
<4>[ 5.870910] mmci-omap-hs.1 supply vmmc_aux not found, using dummy regulator
<6>[ 5.980346] usb 1-2.1: New USB device found, idVendor=0424, idProduct=ec00
<6>[ 5.987548] usb 1-2.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
<6>[ 6.003875] usbcore: registered new interface driver usbhid
<6>[ 6.009704] usbhid: USB HID core driver
<6>[ 6.019653] logger: created 64K log 'log_main'
<6>[ 6.027160] logger: created 256K log 'log_events'
<6>[ 6.032470] smsc95xx v1.0.4
<4>[ 6.042694] mmc1: card claims to support voltages below the defined range. These will be ignored.
<6>[ 6.052825] logger: created 64K log 'log_radio'
<6>[ 6.065887] logger: created 64K log 'log_system'
<6>[ 6.081573] usbcore: registered new interface driver snd-usb-audio
<4>[ 6.090179] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
<6>[ 6.106353] OMAP3 Beagle/Devkit8000 SoC init
<6>[ 6.130340] mmc1: new SDIO card at address 0001
<6>[ 6.169647] smsc95xx 1-2.1:1.0: usb0: register 'smsc95xx' at usb-ehci-omap.0-2.1, smsc95xx USB 2.0 Ethernet, 0a:c3:97:8b:dd:f4
<6>[ 6.194732] asoc: twl4030-hifi <-> omap-mcbsp-dai.1 mapping ok
<6>[ 6.222167] ALSA device list:
<6>[ 6.225280] #0: omap3beagle
<6>[ 6.228393] oprofile: hardware counters not available
<6>[ 6.233703] oprofile: using timer interrupt.
<6>[ 6.238525] TCP cubic registered
<6>[ 6.241912] Initializing XFRM netlink socket
<6>[ 6.246795] NET: Registered protocol family 10
<6>[ 6.252044] lo: Disabled Privacy Extensions
<6>[ 6.256805] Mobile IPv6
<6>[ 6.259399] IPv6 over IPv4 tunneling driver
<6>[ 6.300323] sit0: Disabled Privacy Extensions
<6>[ 6.316009] ip6tnl0: Disabled Privacy Extensions
<6>[ 6.320953] NET: Registered protocol family 17
<6>[ 6.325683] NET: Registered protocol family 15
<6>[ 6.339233] Bluetooth: L2CAP ver 2.15
<6>[ 6.343078] Bluetooth: L2CAP socket layer initialized
<6>[ 6.348419] Bluetooth: SCO (Voice Link) ver 0.6
<6>[ 6.353149] Bluetooth: SCO socket layer initialized
<6>[ 6.370483] Bluetooth: RFCOMM TTY layer initialized
<6>[ 6.375610] Bluetooth: RFCOMM socket layer initialized
<6>[ 6.381011] Bluetooth: RFCOMM ver 1.11
<6>[ 6.384948] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
<6>[ 6.390533] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
<5>[ 6.425415] Registering the dns_resolver key type
<6>[ 6.430389] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
<6>[ 6.448822] ThumbEE CPU extension supported.
<3>[ 6.472656] Power Management for TI OMAP3.
<6>[ 6.496307] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
<6>[ 6.504577] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
<6>[ 6.534515] SmartReflex Class3 initialized
<6>[ 6.542541] clock: disabling unused clocks to save power
<4>[ 6.549041] platform iva.0: omap_voltage_scale: Already at the requestedrate 800000000
<4>[ 6.557312] platform mpu.0: omap_voltage_scale: Already at the requestedrate 1000000000
<4>[ 6.659851] regulator_init_complete: incomplete constraints, leaving VDAC on
<6>[ 6.683563] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
<6>[ 6.692108] omap_vout omap_vout: Buffer Size = 3686400
<6>[ 6.737640] omap_vout omap_vout: : registered and initialized video device 15
<6>[ 6.745086] omap_vout omap_vout: Buffer Size = 3686400
<6>[ 6.761199] omap_vout omap_vout: : registered and initialized video device 16
<6>[ 6.777008] Waiting 2sec before mounting root device...
<5>[ 8.895202] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
<5>[ 8.901458] UBIFS: file system size: 505364480 bytes (493520 KiB, 481 MiB, 3980 LEBs)
<5>[ 8.909820] UBIFS: journal size: 9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
<5>[ 8.917449] UBIFS: media format: w4/r0 (latest is w4/r0)
<5>[ 8.923492] UBIFS: default compressor: lzo
<5>[ 8.927764] UBIFS: reserved for root: 0 bytes (0 KiB)
<4>[ 8.934173] VFS: Mounted root (ubifs filesystem) on device 0:13.
<6>[ 8.940490] Freeing init memory: 224K
<4>[ 9.044158] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
<3>[ 9.377288] init: cannot open '/initlogo.rle'
<3>[ 9.399414] init: cannot find '/system/bin/sgx/rc.pvr', disabling 'pvr'
<3>[ 9.429077] init: cannot find '/system/bin/rild', disabling 'ril-daemon'
<3>[ 9.494873] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
<6>[ 9.761535] Compat-wireless backport release: ol_R5.SP2.04
<6>[ 9.767242] Backport based on wl12xx.git ol_R5.SP2.04
<6>[ 10.286132] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 10.337707] cfg80211: World regulatory domain updated:
<6>[ 10.343109] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 10.351837] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 10.360076] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 10.368469] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 10.376708] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 10.384979] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<3>[ 11.219116] init: using deprecated syntax for specifying property 'sys.usb.config', use ${name} instead
<6>[ 11.297210] enabling adb
<6>[ 11.354949] adb_open
<6>[ 35.447082] warning: `zygote' uses 32-bit capabilities (legacy support in use)
<3>[ 45.798614] init: no such service 'dhcpcd_ip6tnl0'
<3>[ 50.817321] init: no such service 'dhcpcd_ip6tnl0:-h android-d5df27c171264123 ip6tnl0'
<6>[ 50.944427] disabling adb
<6>[ 50.949645] adb_release
<3>[ 51.961944] init: using deprecated syntax for specifying property 'sys.usb.config', use ${name} instead
<6>[ 51.990631] enabling adb
<6>[ 52.007354] adb_open
<3>[ 53.019592] init: using deprecated syntax for specifying property 'sys.usb.config', use ${name} instead
<3>[ 56.844390] binder: release proc 1449, transaction 3076, not freed
<6>[ 61.129791] android_usb gadget: high speed config #1: android
<3>[ 72.692932] init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
<7>[ 111.803833] ieee80211 phy0: Failed to initialize wep: -2
<6>[ 111.810089] wl12xx: loaded
<6>[ 112.021697] wl12xx: state: 0
<6>[ 112.587707] wl12xx: firmware booted (Rev 6.3.9.0.120)
<6>[ 112.629119] ADDRCONF(NETDEV_UP): wlan0: link is not ready
<6>[ 112.763549] wl12xx: state: 2
<6>[ 112.789428] ADDRCONF(NETDEV_UP): p2p0: link is not ready
<7>[ 143.769195] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 143.800109] wlan0: authenticated
<7>[ 143.878448] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 143.882965] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 143.882995] wlan0: associated
<7>[ 143.882995] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 143.882995] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<6>[ 143.911071] ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
<7>[ 144.074188] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 144.074615] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 144.074615] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 144.121459] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 144.230499] cfg80211: World regulatory domain updated:
<6>[ 144.235900] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 144.244781] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 144.253051] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 144.261291] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 144.269561] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 144.277832] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 145.862854] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 145.894927] wlan0: authenticated
<7>[ 145.925506] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 145.971130] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 145.971160] wlan0: associated
<7>[ 145.971191] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 145.971191] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 146.136840] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 146.137268] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 146.137268] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 146.184204] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 146.230651] cfg80211: World regulatory domain updated:
<6>[ 146.236022] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 146.244750] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 146.252990] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 146.261260] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 146.269531] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 146.277770] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 151.730041] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 151.759094] wlan0: authenticated
<7>[ 151.784759] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 151.791870] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 151.791900] wlan0: associated
<7>[ 151.791900] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 151.791931] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 152.042968] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 152.043426] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 152.043457] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 152.097961] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 152.185455] cfg80211: World regulatory domain updated:
<6>[ 152.190887] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 152.199584] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 152.207977] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 152.216217] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 152.224456] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 152.232727] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 155.855224] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 155.884155] wlan0: authenticated
<7>[ 155.909729] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 155.913757] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 155.913787] wlan0: associated
<7>[ 155.913787] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 155.913787] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 156.061248] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 156.063140] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 156.063140] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 156.063262] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 156.121673] cfg80211: World regulatory domain updated:
<6>[ 156.127075] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 156.135803] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 156.144195] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 156.152435] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 156.160705] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 156.168945] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 161.636291] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 161.670288] wlan0: authenticated
<7>[ 161.698760] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 161.703704] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 161.703704] wlan0: associated
<7>[ 161.703735] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 161.703765] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 161.933593] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 161.934204] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 161.934204] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 161.980773] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 162.011383] cfg80211: World regulatory domain updated:
<6>[ 162.016723] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 162.025451] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 162.033691] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 162.041961] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 162.050354] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 162.058593] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 165.816009] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 165.853637] wlan0: authenticated
<7>[ 165.894256] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 165.921936] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 165.921966] wlan0: associated
<7>[ 165.921966] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 165.921966] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 166.105590] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 166.106018] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 166.106018] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 166.152923] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 166.198425] cfg80211: World regulatory domain updated:
<6>[ 166.203826] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 166.212524] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 166.220794] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 166.229034] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 166.237304] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 166.245544] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 171.706604] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 171.735473] wlan0: authenticated
<7>[ 171.776885] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 171.782653] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 171.782684] wlan0: associated
<7>[ 171.782714] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 171.782714] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 172.058593] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 172.059204] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 172.059204] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 172.105773] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 172.144531] cfg80211: World regulatory domain updated:
<6>[ 172.149871] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 172.158630] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 172.166870] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 172.175140] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 172.183532] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 172.191772] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 175.839569] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 175.869750] wlan0: authenticated
<7>[ 175.902008] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 175.908447] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 175.908447] wlan0: associated
<7>[ 175.908477] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 175.908477] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 176.207092] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 176.207550] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 176.207580] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 176.254333] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 176.310089] cfg80211: World regulatory domain updated:
<6>[ 176.315490] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 176.324218] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 176.332489] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 176.340728] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 176.348968] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 176.357238] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 181.808166] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 181.839630] wlan0: authenticated
<7>[ 181.870666] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 181.875030] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 181.875061] wlan0: associated
<7>[ 181.875091] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 181.875091] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 184.214843] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 184.215270] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 184.215301] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 184.261871] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 184.317749] cfg80211: World regulatory domain updated:
<6>[ 184.323150] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 184.331878] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 184.340148] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 184.348388] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 184.356628] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 184.364868] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 186.089508] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 186.122253] wlan0: authenticated
<7>[ 186.152221] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 186.156463] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 186.156494] wlan0: associated
<7>[ 186.156524] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 186.156524] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 186.285980] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 186.287597] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 186.287597] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 186.288879] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 186.317016] cfg80211: World regulatory domain updated:
<6>[ 186.322387] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 186.331115] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 186.339569] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 186.347808] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 186.356048] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 186.364318] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 191.831726] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 191.871398] wlan0: authenticated
<7>[ 191.901916] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 191.909820] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 191.909820] wlan0: associated
<7>[ 191.909851] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 191.909851] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 194.113342] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 194.113769] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 194.113800] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 194.160736] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 194.206695] cfg80211: World regulatory domain updated:
<6>[ 194.212036] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 194.220916] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 194.229156] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 194.237426] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 194.245697] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 194.253936] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 196.073791] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 196.104034] wlan0: authenticated
<7>[ 196.136291] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 196.140319] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 196.140350] wlan0: associated
<7>[ 196.140350] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 196.140380] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 196.402404] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 196.402862] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 196.402862] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 196.449493] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 196.506225] cfg80211: World regulatory domain updated:
<6>[ 196.511657] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 196.520355] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 196.528625] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 196.536865] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 196.545104] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 196.553375] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 202.003479] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 202.035125] wlan0: authenticated
<7>[ 202.065979] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 202.070404] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 202.070434] wlan0: associated
<7>[ 202.070434] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 202.070434] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 202.786102] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 202.786590] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 202.786621] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 202.832336] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 202.887481] cfg80211: World regulatory domain updated:
<6>[ 202.892852] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 202.901580] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 202.909851] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 202.918090] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 202.926361] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 202.934722] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 206.097167] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 206.127960] wlan0: authenticated
<7>[ 206.159881] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 206.163909] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 206.163940] wlan0: associated
<7>[ 206.163940] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 206.163970] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 206.293060] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 206.309906] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 206.309936] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 206.340148] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 206.367736] cfg80211: World regulatory domain updated:
<6>[ 206.373199] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 206.381896] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 206.390167] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 206.398406] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 206.406799] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 206.415039] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 211.933380] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 211.982360] wlan0: authenticated
<7>[ 212.011291] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 212.015350] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 212.015380] wlan0: associated
<7>[ 212.015380] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 212.015411] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 212.136779] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 212.153717] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 212.153717] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
<6>[ 212.183990] cfg80211: Calling CRDA to update world regulatory domain
<6>[ 212.247131] cfg80211: World regulatory domain updated:
<6>[ 212.252502] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>[ 212.261230] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 212.269500] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 212.277740] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>[ 212.285980] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>[ 212.294250] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<7>[ 216.105041] wlan0: authenticate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 216.138366] wlan0: authenticated
<7>[ 216.167541] wlan0: associate with b4:75:0e:1d:05:a7 (try 1)
<7>[ 216.172088] wlan0: RX AssocResp from b4:75:0e:1d:05:a7 (capab=0x411 status=0 aid=8)
<7>[ 216.172119] wlan0: associated
<7>[ 216.172119] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 216.172149] wlan0: moving STA b4:75:0e:1d:05:a7 to state 2
<7>[ 216.433715] wlan0: deauthenticating from b4:75:0e:1d:05:a7 by local choice (reason=1)
<7>[ 216.434143] wlan0: moving STA b4:75:0e:1d:05:a7 to state 1
<7>[ 216.434173] wlan0: moving STA b4:75:0e:1d:05:a7 to state 0
Best Regard !
Hibk