Hi E2E-Community,
we are using a WL1837 with BlueZ 5.30 as bluetooth stack (running on a linux 3.14.42 kernel) and discovered a problem with the currently available firmware from https://git.ti.com/ti-bt/service-packs/trees/master. The problem is, that when A2DP switches from streaming to stopped (no other profile is connected), we discovered a disconnect (reason 1) from the smartphone after exactly 20 seconds. It's only discovered on Android phones so far, using Lollipop and Jelly Bean. No issue on iPhones.
We have already debugged and checked HCI dump and etc. There is nothing showing an indication for an problem on our application side. Not even a visible transfer towards the BlueZ stack.
The problem doesn't occur with an older firmware. (TI_P2.112), but only with the new one (TI_P2.127). Due to that we assume it's because some settings of WiLink8 internally.
Can you help us with this matter? Anyone having the same problems?
Thanks and BR
Elmar