Dear,
I am using the CC3200 in AP mode.
I want to transfer streaming audio signal from PC to CC3200.
So, I need the TCP socket communication for Wi-Fi audio system.
My question is as follows:
1. When CC3200 in AP mode, Would it be possible to communicate TCP or UDP socket.
-> CC3200 TCP socket was implemented as STA mode at example code. but I want to use for AP mode.
2. For audio streaming Wi-Fi system, Which do you recommend TCP of UDP socket communication?
3. If CC3200 support TCP or UDP socket communication in AP mode, does it provide to operate 'server' and 'client' both?
Thanks.
Regards!
Juhee Park.