This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How does I2S Data work in CPU mode?



Hi,

I want to transfer PCM signal to I2S data line.

but, I2S data line is not working.

My source code as follows:

=================================================================

MAP_PRCMPeripheralClkEnable(PRCM_I2S, PRCM_RUN_MODE_CLK);
MAP_PRCMPeripheralReset(PRCM_I2S);

MAP_PRCMI2SClockFreqSet(15360000);  //48000Hz * 2CH * 16Bit

I2SConfigSetExpClk(I2S_BASE, 15360000, 1536000, I2S_SLOT_SIZE_16|I2S_PORT_CPU); //Not used DMA

I2SIntRegister(I2S_BASE, I2SIntHandler);
I2SIntEnable(I2S_BASE, I2S_INT_XDATA);

I2SSerializerConfig(I2S_BASE, I2S_DATA_LINE_0, I2S_SER_MODE_TX, I2S_INACT_LOW_LEVEL);
I2SEnable(I2S_BASE, I2S_MODE_TX_ONLY);

int i=192;
while(i > 0)  //Write 192Byte
{

    I2SDataPut(I2S_BASE, I2S_DATA_LINE_0, 0xFF);
    i--;
}

Thanks,

Juhee Park.