Hello,
I am designing my own PCB based on the CC3200 chip. I would like to include in the PCB only the essential parts to run the firmware, not to program it (cc3200, flash, and power management parts).
In order to program my PCB, I would use the already designed CC3200 Launchpad, using the UART signals (jumpers J6 and J7) and connecting them to my PCB, and then using Uniflash to program it.
Given that I would not use the JTAG connection, the CC3200 chip should include from factory the bootloader needed to use the UART signal to program, as it is included in the CC3200 Launchpad.
Is it possible to do this or the bootloader from factory in CC3200 chip is different from the one in CC3200 Launchpad?
Thank you very much.