While building SmartConfig Source code, it is displaying following error..
ld: warning: ignoring file /Naresh/CC3000_Smartconfig_iOS_Source-1.1/src/CC3x/libFTC_DEBUG_ARM_64.a, missing required architecture x86_64 in file /Naresh/CC3000_Smartconfig_iOS_Source-1.1/src/CC3x/libFTC_DEBUG_ARM_64.a (2 slices)
ld: warning: ignoring file /Naresh/CC3000_Smartconfig_iOS_Source-1.1/src/CC3x/libFTC_RELEASE_ARM_64.a, missing required architecture x86_64 in file /Naresh/CC3000_Smartconfig_iOS_Source-1.1/src/CC3x/libFTC_RELEASE_ARM_64.a (2 slices)
Undefined symbols for architecture x86_64:
"_OBJC_CLASS_$_FirstTimeConfig", referenced from:
objc-class-ref in CC3xUtility.o
objc-class-ref in CC3xMainViewController.o
objc-class-ref in CC3xMainViewController_iPad.o
ld: symbol(s) not found for architecture x86_64
clang: error: linker command failed with exit code 1 (use -v to see invocation)