I adding am335x-bone-cc3100-spi.dtsi file which I got from github.com/.../cc3100-spi-kernelmodul. I have modified the file am335x-boneblack.dts to include this new file and tried to build, but getting the following error message. I have also included the am335x-bone-cc3100-spi.dtsi below.
...
....
CALL scripts/checksyscalls.sh
DTC arch/arm/boot/dts/am335x-bone.dtb
DTC arch/arm/boot/dts/am335x-boneblack.dtb
ERROR (phandle_references): Reference to non-existent node or label "spi0_pins"
ERROR: Input tree has errors, aborting (use -f to force output)
make[1]: *** [arch/arm/boot/dts/am335x-boneblack.dtb] Error 2
make: *** [dtbs] Error 2
jey@ubuntu:~/source_code/BBB/linux-4.1-RN/bb-kernel$
This is the am335x-bone-cc3100-spi.dtsi file:
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/* include this file in am335x-bone.dts */
&ocp {
P9_17_pinmux {
status = "disabled";
};
P9_18_pinmux {
status = "disabled";
};
P9_21_pinmux {
status = "disabled";
};
P9_22_pinmux {
status = "disabled";
};
};
&spi0 {
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins>;
status = "okay";
cc3100 {
compatible = "ti,cc3100";
reg = <0>;
spi-max-frequency = <20000000>;
gpio_nHIB = <39>; //P8_04
gpio_irq= <37>; //P8_22
};
};
Any idea what could be causing this error message?
Thanks.
Jey