This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing CC3200 with GSM Click

Other Parts Discussed in Thread: CC3200

I recently purchased the GSM Click module and have been trying to talk to this board via uart using the CC3200 launch pad, but I was not successful in receiving proper response from the GL865 so far. Has anyone been working on this and could share some experience?

My settings are as follows:

- Connect TX on the GSM Click to UART1-TX (pin 1) on the CC3200

- Connect RX on the GSM Click to UART1-RX (pin 2) on the CC3200

- 3.3V 

Then I have been trying to send AT command using both 115200 and 9600 baud rates to the GL865 but neither baud rate gave me an OK response. In other words, I was sending string "AT\r" over uart and was expecting to see "OK\r" in response but the response always returned with random bytes.

Any help on this would be greatly appreciated.