Hi All,
We have implemented the WiFi direct communicating between one CC3200 module and android device.
For implementing this I have used P2P application from CC3200 SDK with CC3200 launchpad only. The CC3101 SDK does not have P2P application.
1) I want to know whether it is possible to do WiFi direct communication between two CC3200 modules.
2) Also the CC3200 SDK is not loading the application after flashing .bin file using slprogrammer. But if we use the same slprogrammer for CC3101 SDK it is loading the application after flashing the .bin file.
Kindly assist me on solving the above issues.
Thanking you,
-Yasar Arafath.