This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200SDK_1.1.0 Known Issues : Pin #17 driven high during hibernate when device in SOP mode "Fn2WJ" .



Hi All,

Please note that a new known issue has been added for SDK 1.1.0 in the link below

processors.wiki.ti.com/.../CC32xx_Summary_of_Known_Issues

Issue Description:

Pkg Pin #17 (Pin Alias TDO) is driven high during hibernate when device is operating in SOP mode "Fn2WJ(Functional mode with a 2-wire SWD mapped to fixed pins)". If this pin is used to connect some other device which has a conflicting drive then there could be current leakage in hibernate mode.

For further details refer to Issue #3 @ http://processors.wiki.ti.com/index.php/CC32xx_Summary_of_Known_Issues#Pinmux_changes  

Thanks and Regards,

Siddaram