Hi
We are using the CC3100MOD with spi Interface to AM335X processor. We are using linux kernel.
For testing we are using the CC3200/3100 SDK "spi_test_tool", together with rpricken/cc3100-linux kernel driver.
Problem:
When sending the init command we don't get any answer on the MISO line.
Command:
TX: 0x65 0x87 0x78 0x56
RX: 0x0 0x0 0x0 0x0
RX: 0x0 0x0 0x0 0x0
RX: 0x0 0x0 0x0 0x0
(I have tried the same on a beaglebone black card connected to CC3100MODBOOST and the code are working.
Schematic of the CC3100MOD on our card.
I have connected my computer with "CCS Uniflash" on the UART interface and program gives me information/respons from the CC3100 module. I can also connect to it in AP mode with my Telephone.
Why don't i get any respons from the cc3100MOD chip on the MISO line ?
I hope that someone can guide me to solve this problem.
ASN