Hi,
I want to check the feasibility for following functionalities:
- Have to capture and send video + Audio from camera (540p pr 720p with 30fps will be enough) via WiFi to external network and to Mobile
- From Mobile Audio will be transmitted back to Processor and to speaker.
- Latency should not be more than 200 ms.(This is must)
- There might be some proximity or motion or light sensor and switch interfaces.
- Want to avoid Processors with BGA packages.(Not a must but can trade off)
- Last but not least not expensive (including camera)
I will like to have some Evaluation Kit to do Feasibility and Performance analysis. What is a good Processor to achieve this? Any idea or guideline from where to start development?
Thanks in advance.