I am using a CC3200MOD board DIY and try to program this board by using uniflash via CC3200launchxl.
I try to connect as this processors.wiki.ti.com/.../CC3200MOD_Production_Line_Guide
Launchxl - My DIY board
P57 - GPIO1
P55 - GPIO2
nRST - nRST
GND - GND
SOP2 in my DIY board is connected to 3.3v
Baudrate is 921600.
I get this error
[20:07:45] INFO: > Executing Operation: Connect [20:07:47] INFO: setting break signal [20:07:48] INFO: detecting FTDI for device reset [20:08:04] ERROR: ---reading ACK signal failed--- [20:08:04] WARNING: ---seting break signal to false failed--- [20:08:06] INFO: setting break signal [20:08:07] INFO: detecting FTDI for device reset [20:08:22] ERROR: ---reading ACK signal failed--- [20:08:22] WARNING: ---seting break signal to false failed--- [20:08:24] INFO: setting break signal [20:08:25] INFO: detecting FTDI for device reset [20:08:41] ERROR: ---reading ACK signal failed--- [20:08:41] WARNING: ---seting break signal to false failed--- [20:08:43] INFO: setting break signal [20:08:44] INFO: detecting FTDI for device reset [20:08:59] ERROR: ---reading ACK signal failed--- [20:08:59] WARNING: ---seting break signal to false failed--- [20:08:59] FATAL: --- Can't connect to device !! --- [20:08:59] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3 [20:08:59] INFO: > Executing Operation: Disconnect [20:08:59] Operation Format returned.
Could anyone help me to solve this problem? Thanks!