Hello All,
I have a setup of following..
1. Host PC (Macbook Pro) where a TCP/IP server application is running
2. CC3200 device as client
Both Host PC and CC3200 device are connected over common Wi-Fi access point (TP Link Wi-Fi access point).
CC3200 device programming is done using Energia Sketch programs.
CC3200 device is able to connect with host PC application by using Host PC IP address. All is good and working.
Problem:
If CC3200 device is asked to resolve IP address using host PC network name, it is unable to resolve. However CC3200 device is able to resolve standard websites such as Google and Facebook.
I am not sure, what could be the problem and any help on this will be greatly appreciated.
Thanks,
Ajit B