Hello!
Does the CC3200 support SNI on the client?
https://en.wikipedia.org/wiki/Server_Name_Indication
Thanks for the help!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
Does the CC3200 support SNI on the client?
https://en.wikipedia.org/wiki/Server_Name_Indication
Thanks for the help!
Hello,
The mentioned thread refers to CC3100, but I assume the informatin in ii is valid for CC3200 as well; in this case, could you confirm that a new CC3200 hardware version will be needed to have SNI support? And is there a timeline for such support?
Thank you
Hi Francesco,
I think that there was a misunderstanding in the SNI requirement.
This feature is used in order to connect different host servers on the same port - it's not planned to be supported.
The confusion came from the feature we added to SDK1.2 to verify the domain server name.
I'm sorry for this confusion.
Best Regards,
Nir Nitzani
Same question here. I have a CC3200 project, and I cannot connect to AWS API Gateway using a custom domain name that requires SNI. The HTTPCli_connect API returns -102 despite having a valid root certificate file. Does the latest CC3200 SDK support SNI? If not, when?
Thanks,
Clinton Knight
Hi Clinton,
Answer at 2nd post is clear (https://e2e.ti.com/support/wireless_connectivity/simplelink_wifi_cc31xx_cc32xx/f/968/t/422647). There is not planned to add SNI support into CC3200. From that answer I am not sure, but also it looks that SNI will not be supported at new CC3220.
Jan