Hello,
I'm midway through prototyping, and have only just discovered that the CC3100MOD can only support a single Client Station Connection.
I suppose I should start with my intended use case. The product is a battery powered Wireless Sensor Network, first deployment being 300 - 400 units.
We were going to use 8 slave sensor boards, which would each connect to a node board. The sensor slaves would gather sensor data, format it, connect to a node board via WiFi in Access Point mode, then sleep for a period of time. The node boards would in turn connect to a Gateway Master board via WiFi in Access Point mode, backup data to SD Card, and use an Ethernet connection to communicate with a remote dashboard and database.
With only 1 Station connection allowed, it seems that this would be impossible. Please advise to a solution, workaround, or even another SimpleLink product offering that would be viable. We would like to maintain the CC3100MOD as our module of choice, but will use another product if need be.
Are there any current reference designs that may help? Would Transceiver mode allow this use case?
I'm in quite a bit of a pit with this, all other development has stopped on this project, so any pointers, links, tips, etc would be very much appreciated. It had seemed at first glance that the CC3100MOD would fit the bill -perfectly-, our team only wishes it was stated more clearly the "One Station Connection in AP Mode" limitation... We would have never come this far had that been known at the time.
Is it possible to code on top of the driver code, to allow more than the one connection?
The deployment is for an industrial setting, not our own building. Our product is meant to be installed at this remote industrial location, and putting up third party Access Points would be quite unprofessional, maybe even laughable. How can a wireless sensor network of this type -not- be expected to be all-inclusive with regards to Connection Topology? I hope the suggested answer doesn't come to "Oh, just install an Access Point in place of each Node Board." For 360 sensor boards, that comes out to 45 separate third party Access Points. This is a three story, nearly mile long warehouse. This would remove all agency of our product to be a fully autonomous Sensor Network...
Please advise, we're really pulling for you on this TI...