I'm trying to build the uart_demo project specifically, but really all of them have this problem. When I try to compile I get a linker warning:
warning #10207-D: automatic RTS selection: resolving index library "libc.a" to "rtsv7M4_T_le_eabi.lib", but "rtsv7M4_T_le_eabi.lib" was not found
warning #10062-D: entry-point symbol "_c_int00" undefined
And a compilation error:
>> Compilation failure
undefined first referenced
symbol in file
--------- ----------------
__STACK_END ./startup_ccs.ob
error #10234-D: unresolved symbols remain
warning #10202-D: no suitable entry-point found; setting to 0
error #10010: errors encountered during linking; "uart_demo.out" not built
I've done some searching and seen that people have noticed this as a Cygwin issue, but I don't have Cygwin installed on this computer anymore. Cygwin doesn't show up in my path or in the registry. Could it be something else? How do I go about debugging this?
Thanks