Hi,
i'm clearly missing something here. My SD card is working without problems using following pin configuration:
// // Configure PIN_06 for SDHost0 SDCARD_DATA // PinTypeSDHost(PIN_06, PIN_MODE_8); // // Configure PIN_07 for SDHost0 SDCARD_CLK // PinTypeSDHost(PIN_07, PIN_MODE_8); // // Configure PIN_08 for SDHost0 SDCARD_CMD // PinTypeSDHost(PIN_08, PIN_MODE_8); // // Set the SD card clock as output pin // MAP_PinDirModeSet(PIN_07, PIN_DIR_MODE_OUT); // // Enable Pull up on data // MAP_PinConfigSet(PIN_06, PIN_STRENGTH_4MA, PIN_TYPE_STD_PU); // // Enable Pull up on CMD // MAP_PinConfigSet(PIN_08, PIN_STRENGTH_4MA, PIN_TYPE_STD_PU);
But if i change PIN 07 to PIN 01 as suggested by pinmux tool it stops working:
// // Configure PIN_01 for SDHost0 SDCARD_CLK // PinTypeSDHost(PIN_01, PIN_MODE_6);
Is it possible to use PIN 01 as SDHost CLK while connected via USB? Or maybe there is a problem with the onboard LED?
Hopefully someone can point me in the right direction. Thanks in advance!
My full pinmux config if it matters:
// // Enable Peripheral Clocks // PRCMPeripheralClkEnable(PRCM_GPIOA0, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_GPIOA1, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_GPIOA2, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_GPIOA3, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_SDHOST, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_GSPI, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_UARTA0, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_UARTA1, PRCM_RUN_MODE_CLK); PRCMPeripheralClkEnable(PRCM_I2CA0, PRCM_RUN_MODE_CLK); // // Configure PIN_50 for GPIO Output // PinTypeGPIO(PIN_50, PIN_MODE_0, false); GPIODirModeSet(GPIOA0_BASE, 0x1, GPIO_DIR_MODE_OUT); // // Configure PIN_58 for GPIO Input // PinTypeGPIO(PIN_58, PIN_MODE_0, false); GPIODirModeSet(GPIOA0_BASE, 0x8, GPIO_DIR_MODE_IN); // // Configure PIN_59 for GPIO Input // PinTypeGPIO(PIN_59, PIN_MODE_0, false); GPIODirModeSet(GPIOA0_BASE, 0x10, GPIO_DIR_MODE_IN); // // Configure PIN_60 for GPIO Input // PinTypeGPIO(PIN_60, PIN_MODE_0, false); GPIODirModeSet(GPIOA0_BASE, 0x20, GPIO_DIR_MODE_IN); // // Configure PIN_61 for GPIO Input // PinTypeGPIO(PIN_61, PIN_MODE_0, false); GPIODirModeSet(GPIOA0_BASE, 0x40, GPIO_DIR_MODE_IN); // // Configure PIN_62 for GPIO Output // PinTypeGPIO(PIN_62, PIN_MODE_0, false); GPIODirModeSet(GPIOA0_BASE, 0x80, GPIO_DIR_MODE_OUT); // // Configure PIN_63 for GPIO Output // PinTypeGPIO(PIN_63, PIN_MODE_0, false); GPIODirModeSet(GPIOA1_BASE, 0x1, GPIO_DIR_MODE_OUT); // // Configure PIN_64 for GPIO Output // PinTypeGPIO(PIN_64, PIN_MODE_0, false); GPIODirModeSet(GPIOA1_BASE, 0x2, GPIO_DIR_MODE_OUT); // // Configure PIN_15 for GPIO Input // PinTypeGPIO(PIN_15, PIN_MODE_0, false); GPIODirModeSet(GPIOA2_BASE, 0x40, GPIO_DIR_MODE_IN); // // Configure PIN_18 for GPIO Input // PinTypeGPIO(PIN_18, PIN_MODE_0, false); GPIODirModeSet(GPIOA3_BASE, 0x10, GPIO_DIR_MODE_IN); // // Configure PIN_21 for GPIO Output // PinTypeGPIO(PIN_21, PIN_MODE_0, false); GPIODirModeSet(GPIOA3_BASE, 0x2, GPIO_DIR_MODE_OUT); // // Configure PIN_53 for GPIO Input // PinTypeGPIO(PIN_53, PIN_MODE_0, false); GPIODirModeSet(GPIOA3_BASE, 0x40, GPIO_DIR_MODE_IN); // // Configure PIN_06 for SDHost0 SDCARD_DATA // PinTypeSDHost(PIN_06, PIN_MODE_8); // // Configure PIN_01 for SDHost0 SDCARD_CLK // PinTypeSDHost(PIN_01, PIN_MODE_6); // // Configure PIN_08 for SDHost0 SDCARD_CMD // PinTypeSDHost(PIN_08, PIN_MODE_8); // // Configure PIN_45 for SPI0 GSPI_CLK // PinTypeSPI(PIN_45, PIN_MODE_7); // // Configure PIN_07 for SPI0 GSPI_MOSI // PinTypeSPI(PIN_07, PIN_MODE_7); // // Configure PIN_03 for UART0 UART0_TX // PinTypeUART(PIN_03, PIN_MODE_7); // // Configure PIN_57 for UART0 UART0_RX // PinTypeUART(PIN_57, PIN_MODE_3); // // Configure PIN_55 for UART1 UART1_TX // PinTypeUART(PIN_55, PIN_MODE_6); // // Configure PIN_02 for UART1 UART1_RX // PinTypeUART(PIN_02, PIN_MODE_7); // // Configure PIN_05 for I2C0 I2C_SCL // PinTypeI2C(PIN_05, PIN_MODE_5); // // Configure PIN_04 for I2C0 I2C_SDA // PinTypeI2C(PIN_04, PIN_MODE_5);