Hi,
I updated the CC3100 module to the above mentioned new ServicePack (1. Format, Then flash Service Pack). Then I updated the Host driver on the controller to the one from SDK 1.2.0.
Now the initialization of CC3100 seems to work but after that the CC3100 does not answer anymore.
Here is a screenshot of the CC3100 interface:
This is zoomed at 7ms where the interrupt from CC3100 is asserted:
And here is the communication part after the irq. The SYNC pattern is send but CC3100 does not answer.
Any ideas what can be wrong here?
Regards
Simon