Hello,
I would like to know if it is possible to connect the WL1837MOD module to the BeagleBone Black board and, at the same time, boot from the eMMC and use the uSD card as storage device.
Thank you very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alessandro,
Yes, the uSD can be used for everything, so I don't think it is a real limitation other than the fact that the EMMC is just not used.
It is used for booting and root file system with full R/W. The same as the emmc qouls have been used.
Best Regards,
Eyal
Jonatan thanks for the suggestion.
The Beaglebone Green Wireless has not the eMMC problem, but the Wi-Fi frequency is fixed at 2.4GHz. Is it correct?