Hi,
I am planning to use the CC3100MOD part in a new design. As I understand, it is pre-certified. I have the following questions regarding the use of the CC3100MOD:
1. In my design I cannot use an on-board antenna (device will be mounted in RF-opaque metal box). Instead, the BG-RF pad of the module will be connected to a board-edge SMA connector (50 Ohm), connected via 1ft coax cable (50 Ohm) to a duck antenna (50 Ohm). As the trace length between BG-RF and SMA connector is only ~1.6mm, do I need an impedance matching circuit? IMHO the additional trace lengths required for the impedance matching circuit might actually be themselves the cause for needing it in the first place.
2. Does the TI WIFI certifications only apply if a board mounted antenna is used, or does it apply also if the antenna used does not have a higher gain than the board-mounted chip antenna?
3. Does the CC3100MOD part come pre-flashed with a (preferably latest) service pack?
4. In my design I have a spare UART in the main MCU (ATMEL SAMS70) that could be used for the format flash function of the CC3100MOD for field upgrades. However, I cannot provide an exact baud rate of 921600. The nearest I can provide is 937500, which is 1.7% faster. Is this within spec for the CC3100?
5. The CC3100MOD datasheet only mentions to provide ground vias under the module for thermal reasons. Is there a spec on how many are needed for thermal reasons? I do have a solid ground pad under the module. Do I need to provide for thermal conductance to the back of my PCB?
Additional note:
The Production line guides for CC3100MOD and CC3100 have a drawing for how to connect a CC31XXEMOBOOST board to either a CC3100QFN or CC3100MOD TX/RX. Specifically it says to connect P1.3 to UART-RX of the CC3100(MOD) and P1.4 to UART-TX. However, the schematic of CC3100BOOST Rev4 shows P1.3 to be connected to UART-TX of the CC3100 and P1.4 connected to UART-RX of the CC3100. I verified the schematic to be correct. Therefore the production line guides are both wrong. In addition, the production line guides do not show a ground reference connection (P3.2). Without that using the described procedure does not work.