Hi all,
I'm doing a project for my masters on finding the optimum time to send a packet from a vehicle to a road side unit (RSU).
I have two Ti MSP430FR6989 and CC3100 with the advanced emulation booster pack.
I've managed to set the MSP430 and the CC3100 up as a server using the SimpleWiFIServer example in Energia. I used my phone as the AP. I then tried to incorporate the network and the server onto the MSP430 and CC310, similar to the out of box example. This didn't work for me.
At a high level I believe all I need to set up is a P2P network that will allow me to send/receive data so I can calculate the frame error rate and measure the RSSI. The part I am struggling with the P2P network .
Any help or pointers would be greatly appreciated.
Regards,
Ciaran