This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

red LED D7 blinking at wlan_station

Other Parts Discussed in Thread: CC3200

Hi,

for some reason I can't connect to AP with the launch pad CC3200 even when ALL parameters are OK.

When tried a couple of days ago it worked OK but then I tried to set static IP and from that point connection went wrong (BTW, setting static IP is not simple for HW field guy, there is no documention and it involves C++ qualification..)

Anyway, when building the wlan_station example, after setting the common.h file correctly, and bringing back the DHCP enable option (which was the only way that it worked for me) I still don't get the full message on the Tera Terminal which indicates the CC3200 got its IP address.

Any ideas? is there's any way to know on which state/ip address the board in?

THX