This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding advertisement of device

Hi,
I have successfully compiled linux add on package for my set up using yocto and everthing works fine.
I want to know that can i connect more than one mobile phone at a time??
For ex--
When i ran binary LinuxGATM_SRV and advertise using this command StartAdvertising 0x676 100 62C9608E4F9B,it successfully advertised and scanned by mobile phone and when i connect to it, it is connected successfully but it stops advertising 

GATM>
Local Device Properties Changed.
Device Flags: 0xC0000000
LE Scan Mode: FALSE, 0x00000000
LE Adv Mode: FALSE, 0x00000000
LE Slv Mode: In Slave Mode
GATM>
LE Advertising Stopped.
GATM>
GATT Connection Event
Connection Type: LE
Remote Address: 7B53B6317F19
MTU: 23

so is there any way to start advertisement?