Hi,
How to enable the CCA in Wilink8 based system?
Thanks
BR. Albin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Albin,
CCA is on by default as part of 802.11 MAC/PHY. What are you trying to achieve?
Iain
Hi Iain,
Customer is doing below ETSI testing. and got failing.
do you think WiFi should be applied for this clause or CCA could help?
4.3.2.6 Adaptivity (adaptive equipment using modulations other than FHSS)
4.3.2.6.1 Applicability
This requirement does not apply to non-adaptive equipment or adaptive equipment operating in a non-adaptive mode
providing the equipment complies with the requirements and/or restrictions applicable to non-adaptive equipment.
BR. Albin
Hi ALbin,
The settings required for the EN300328 and 301893 are found in the annexe E and F documents linked to from
These give the declarations to the test house which drive which tests to run.
Iain
Hi Albin,
The ETSI tests require the device to be declared as a load based device. This implicitly includes CCA and so disabling CCA is not the solution to the problem.
p) Adaptivity (Channel Access Mechanism): Load Based Equipment Option A
Specify which protocol has been implemented: IEEE 802.11
CCA observation time NA
q) The CCA time implemented by the equipment: 9µs
Hopefully someone else can give the test commands used as this is not something I know.
Iain
Dear Lain and Albin
We have not passed "4.3.2.6 Adaptivity Test" on ETSI testing yet.
In order to verify that Energy Detect is working correctly,
we injected the transmit power of the transmitter against the wl1837 module.
I will attach a log by using WL glogger.
Please find the attached log.
We acquired the log from the injection of jamming waves until the Tx Stop due to jamming waves on wl1837 module.
JammingTest_glogger_2016_11_30.zip
Can you see that the Energy Detect function is working on this log?
I want to know whether Energy Detection is working properly.
Is there a way to know something?
Best regards,
Ryo Goto
Hi Goto Ryo,
using the configuration file for our product with no changes, the CCA is automatically on. This will set the default CCA energy threshold to -72dBm, which is what our product is certified with.
BR. Albin
Hi it should be
- claim file file:///C:/Users/a0389173/Downloads/ETSI_300_328_v191_AnnexE%20(2).pdf
- and the wlconf
BR. Albin
Hi Albin,
As additional information, we will send our current "wl18xx-conf.bin" and "wl18xx-conf.txt".
Please find the attached zip file.
As a base INI file, We use "WL1837MOD_INI_FCC_CE_JP.ini" .
Using "WL1837MOD_INI_FCC_CE_JP.ini", the setting is changed to MIMO and 2.4GHz only.
And we created "wl18xx-conf.bin"
The "wl18xx-conf.txt" is printing a dump file of the"wl18xx-conf.bin" into a text file.
BR Goto
Dear Ryo,
small update: we've passed the CCA testing by lowering TX power, to create more margin in the CCA switch-off threshold (ETSI 1.8)
There will be a FW update from TI somewhere in the coming month(s) (to address ETSI 2.1).
BR, Thomas