Hello
I'm using a Altera Cyclone 5 (HPS) with kernel 4.1.22-ltsi-altera and yoctoproject release morty.
Booting with the WL1837MODCOM8I connected, results in following errors:
[ 1.656969] wl18xx_driver wl18xx.0.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2 [ 1.657010] wl18xx_driver wl18xx.0.auto: Direct firmware load for ti-connectivity/wl18xx-conf.bin failed with error -2 [ 1.657015] wlcore: ERROR could not get configuration binary ti-connectivity/wl18xx-conf.bin: -2 [ 1.657017] wlcore: WARNING falling back to default config ... [ 1.888084] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11) [ 1.897368] wlcore: loaded ... [ 12.561339] wlcore: PHY firmware version: Rev 8.2.0.0.237 [ 12.660168] wlcore: firmware booted (Rev 8.9.0.0.70)
The w18xx-conf.bin was created with configure-device.sh under /usr/sbin/wlconf.
The wl18xx-fw-4.bin and all the tools are from the TI git tag R8.7_SP1.
root@cyclone5:/lib/firmware/ti-connectivity# ls wl18xx-conf.bin wl18xx-fw-4.bin
Is there a solution for this problem?
Best regards
Rico Ganahl
Edit: Thank you for your reply. Try to fix ugly formating of post...