Customer reporting a NULL pointer dereference error with Wilink8 R8.6 on ProcessorSDK 1.03 on AM335x on their own hardware.
It involves a call to cfg80211_prepare_cqm() with the first argument ‘dev’ (R0) being null. dev comes from sdata->dev in ieee80211_cqm_rssi_notify() and sdata comes from vif_to_sdata(vif). vif is passed in from wlcore_event_rssi_trigger() which is an interrupt handler. vif there comes from wl12xx_for_each_wlvif_sta(wl, wlvif).
Anyone seen this error before? How to debug?
Initial error below (can provide full dmesg if needed).
[1912400.918442] wlan0: deauthenticated from 4c:60:de:fd:55:c6 (Reason: 7=CLASS3_FRAME_FROM_NONASSOC_STA)
[1912400.978910] cfg80211: Calling CRDA to update world regulatory domain
[1912401.048290] Unable to handle kernel NULL pointer dereference at virtual address 000001ac
[1912401.057033] pgd = c0004000
[1912401.060067] [000001ac] *pgd=00000000
[1912401.064048] Internal error: Oops: 17 [#1] ARM
[1912401.068813] Modules linked in: usb_f_ecm g_ether usb_f_rndis libcomposite u_ether wl18xx(O) wlcore(O) mac80211(O) cfg80211(O) wakeup_source sync_out....wlcore_sdio(O) compat(O) ir
[1912401.090128] CPU: 0 PID: 1434 Comm: irq/175-wl18xx Tainted: G W O 3.14.43+ #5
[1912401.098458] task: c428d880 ti: c5fc4000 task.ti: c5fc4000
[1912401.104449] PC is at cfg80211_prepare_cqm+0x10/0x148 [cfg80211]
[1912401.110857] LR is at cfg80211_cqm_rssi_notify+0x28/0x7c [cfg80211]
[1912401.117486] pc : [<bf0491e8>] lr : [<bf04d6c4>] psr: 600f0113
[1912401.117486] sp : c5fc5d98 ip : c5fc5dc8 fp : c5fc5dc4
[1912401.129821] r10: c40b7d40 r9 : bf114e7c r8 : c40e5360
[1912401.135449] r7 : 00000002 r6 : 000000d0 r5 : c40e5480 r4 : 00000001
[1912401.142436] r3 : 00000000 r2 : 000000d0 r1 : 00000000 r0 : 00000000
[1912401.149427] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[1912401.157299] Control: 10c5387d Table: 85da0019 DAC: 00000015
[1912401.163529] Process irq/175-wl18xx (pid: 1434, stack limit = 0xc5fc4238)
[1912401.170761] Stack: (0xc5fc5d98 to 0xc5fc6000)
[1912401.175532] 5d80: c5fc5dcc c5fc5da8