Other Parts Discussed in Thread: CC3200
Hi,
I'm communicating 2 -CC3200 launchpad in which 1 working as Transmitter and other working as a receiver and send same data over MQTT server.
CC3200 as Transmitter-
I'm sending Hex values like this-
while(1)
{
char buffer[6]={0xF8,0x1A,0xAB,0X45,0xCC,0x88};
Message(buffer);
}
For Receiver - I'm using MQTT Client project in which i have to get the data from UART and send it to the server(i.e whenever data comes).But I'm not getting hex values & here I'm using UART1 for recieving the data..Below is my code-
#include <stdlib.h>
// simplelink includes
#include "simplelink.h"
// driverlib includes
#include "hw_types.h"
#include "hw_ints.h"
#include "hw_memmap.h"
#include "interrupt.h"
#include "rom_map.h"
#include "prcm.h"
#include "uart.h"
#include "timer.h"
// common interface includes
#include "network_if.h"
#ifndef NOTERM
#include "uart_if.h"
#endif
#include "button_if.h"
#include "gpio_if.h"
#include "timer_if.h"
#include "common.h"
#include "utils.h"
#include "sl_mqtt_client.h"
// application specific includes
#include "pinmux.h"
#define APPLICATION_VERSION "1.1.1"
/*Operate Lib in MQTT 3.1 mode.*/
#define MQTT_3_1_1 false /*MQTT 3.1.1 */
#define MQTT_3_1 true /*MQTT 3.1*/
#define WILL_TOPIC "Client"
#define WILL_MSG "Client Stopped"
#define WILL_QOS QOS2
#define WILL_RETAIN false
/*Defining Broker IP address and port Number*/
#define SERVER_ADDRESS "my server address"
#define PORT_NUMBER 1883
#define MAX_BROKER_CONN 1
#define SERVER_MODE MQTT_3_1
/*Specifying Receive time out for the Receive task*/
#define RCV_TIMEOUT 30
/*Background receive task priority*/
#define TASK_PRIORITY 3
/* Keep Alive Timer value*/
#define KEEP_ALIVE_TIMER 25
/*Clean session flag*/
#define CLEAN_SESSION true
/*Retain Flag. Used in publish message. */
#define RETAIN 1
/*Defining Publish Topic*/
#define PUB_TOPIC_FOR_SW3 "/cc3200/ButtonPressEvtSw3"
#define PUB_TOPIC_FOR_SW2 "/cc3200/ButtonPressEvtSw2"
/*Defining Number of topics*/
#define TOPIC_COUNT 3
/*Defining Subscription Topic Values*/
#define TOPIC1 "/cc3200/ToggleLEDCmdL1"
#define TOPIC2 "/cc3200/ToggleLEDCmdL2"
#define TOPIC3 "/cc3200/ToggleLEDCmdL3"
#define CONSOLE UARTA0_BASE
#define CONSOLE1 UARTA1_BASE
#define UartGetChar() MAP_UARTCharGet(CONSOLE)
#define UartPutChar(c) MAP_UARTCharPut(CONSOLE,c)
#define UartGetChar1() MAP_UARTCharGet(CONSOLE1)
#define UartPutChar1(c) MAP_UARTCharPut(CONSOLE1,c)
/*Defining QOS levels*/
#define QOS0 0
#define QOS1 1
#define QOS2 2
/*Spawn task priority and OSI Stack Size*/
#define OSI_STACK_SIZE 2048
#define UART_PRINT Report
typedef struct connection_config{
SlMqttClientCtxCfg_t broker_config;
void *clt_ctx;
unsigned char *client_id;
unsigned char *usr_name;
unsigned char *usr_pwd;
bool is_clean;
unsigned int keep_alive_time;
SlMqttClientCbs_t CallBAcks;
int num_topics;
char *topic[TOPIC_COUNT];
unsigned char qos[TOPIC_COUNT];
SlMqttWill_t will_params;
bool is_connected;
}connect_config;
typedef enum
{
PUSH_BUTTON_SW2_PRESSED,
PUSH_BUTTON_SW3_PRESSED,
BROKER_DISCONNECTION
}events;
typedef struct
{
void * hndl;
events event;
}event_msg;
//*****************************************************************************
// LOCAL FUNCTION PROTOTYPES
//*****************************************************************************
static void
Mqtt_Recv(void *app_hndl, const char *topstr, long top_len, const void *payload,
long pay_len, bool dup,unsigned char qos, bool retain);
static void sl_MqttEvt(void *app_hndl,long evt, const void *buf,
unsigned long len);
static void sl_MqttDisconnect(void *app_hndl);
void pushButtonInterruptHandler2();
void pushButtonInterruptHandler3();
void ToggleLedState(ledEnum LedNum);
void TimerPeriodicIntHandler(void);
void LedTimerConfigNStart();
void LedTimerDeinitStop();
void BoardInit(void);
static void DisplayBanner(char * AppName);
void MqttClient(void *pvParameters);
//*****************************************************************************
// GLOBAL VARIABLES -- Start
//*****************************************************************************
#ifdef USE_FREERTOS
#if defined(ewarm)
extern uVectorEntry __vector_table;
#endif
#if defined(ccs)
extern void (* const g_pfnVectors[])(void);
#endif
#endif
unsigned short g_usTimerInts;
/* AP Security Parameters */
SlSecParams_t SecurityParams = {0};
/*Message Queue*/
OsiMsgQ_t g_PBQueue;
/* connection configuration */
connect_config usr_connect_config[] =
{
{
{
{
SL_MQTT_NETCONN_URL,
SERVER_ADDRESS,
PORT_NUMBER,
0,
0,
0,
NULL
},
SERVER_MODE,
true,
},
NULL,
"user1",
NULL,
NULL,
true,
KEEP_ALIVE_TIMER,
{Mqtt_Recv, sl_MqttEvt, sl_MqttDisconnect},
TOPIC_COUNT,
{TOPIC1, TOPIC2, TOPIC3},
{QOS2, QOS2, QOS2},
{WILL_TOPIC,WILL_MSG,WILL_QOS,WILL_RETAIN},
false
}
};
/* library configuration */
SlMqttClientLibCfg_t Mqtt_Client={
1882,
TASK_PRIORITY,
30,
true,
(long(*)(const char *, ...))UART_PRINT
};
/*Publishing topics and messages*/
const char *pub_topic_sw2 = PUB_TOPIC_FOR_SW2;
const char *pub_topic_sw3 = PUB_TOPIC_FOR_SW3;
char *data_sw2=buffer;
void *app_hndl = (void*)usr_connect_config;
//*****************************************************************************
// GLOBAL VARIABLES -- End
//*****************************************************************************
//****************************************************************************
//! Defines Mqtt_Pub_Message_Receive event handler.
//! Client App needs to register this event handler with sl_ExtLib_mqtt_Init
//! API. Background receive task invokes this handler whenever MQTT Client
//! receives a Publish Message from the broker.
//!
//!\param[out] topstr => pointer to topic of the message
//!\param[out] top_len => topic length
//!\param[out] payload => pointer to payload
//!\param[out] pay_len => payload length
//!\param[out] retain => Tells whether its a Retained message or not
//!\param[out] dup => Tells whether its a duplicate message or not
//!\param[out] qos => Tells the Qos level
//!
//!\return none
//****************************************************************************
static void
Mqtt_Recv(void *app_hndl, const char *topstr, long top_len, const void *payload,
long pay_len, bool dup,unsigned char qos, bool retain)
{
char *output_str=(char*)malloc(top_len+1);
memset(output_str,'\0',top_len+1);
strncpy(output_str, (char*)topstr, top_len);
output_str[top_len]='\0';
if(strncmp(output_str,TOPIC1, top_len) == 0)
{
ToggleLedState(LED1);
}
else if(strncmp(output_str,TOPIC2, top_len) == 0)
{
ToggleLedState(LED2);
}
else if(strncmp(output_str,TOPIC3, top_len) == 0)
{
ToggleLedState(LED3);
}
UART_PRINT("\n\rPublish Message Received");
UART_PRINT("\n\rTopic: ");
UART_PRINT("%s",output_str);
free(output_str);
UART_PRINT(" [Qos: %d] ",qos);
if(retain)
UART_PRINT(" [Retained]");
if(dup)
UART_PRINT(" [Duplicate]");
output_str=(char*)malloc(pay_len+1);
memset(output_str,'\0',pay_len+1);
strncpy(output_str, (char*)payload, pay_len);
output_str[pay_len]='\0';
UART_PRINT("\n\rData is: ");
UART_PRINT("%s",(char*)output_str);
UART_PRINT("\n\r");
free(output_str);
return;
}
//****************************************************************************
//! Defines sl_MqttEvt event handler.
//! Client App needs to register this event handler with sl_ExtLib_mqtt_Init
//! API. Background receive task invokes this handler whenever MQTT Client
//! receives an ack(whenever user is in non-blocking mode) or encounters an error.
//!
//! param[out] evt => Event that invokes the handler. Event can be of the
//! following types:
//! MQTT_ACK - Ack Received
//! MQTT_ERROR - unknown error
//!
//!
//! \param[out] buf => points to buffer
//! \param[out] len => buffer length
//!
//! \return none
//****************************************************************************
static void
sl_MqttEvt(void *app_hndl, long evt, const void *buf,unsigned long len)
{
int i;
switch(evt)
{
case SL_MQTT_CL_EVT_PUBACK:
UART_PRINT("PubAck:\n\r");
UART_PRINT("%s\n\r",buf);
break;
case SL_MQTT_CL_EVT_SUBACK:
UART_PRINT("\n\rGranted QoS Levels are:\n\r");
for(i=0;i<len;i++)
{
UART_PRINT("QoS %d\n\r",((unsigned char*)buf)[i]);
}
break;
case SL_MQTT_CL_EVT_UNSUBACK:
UART_PRINT("UnSub Ack \n\r");
UART_PRINT("%s\n\r",buf);
break;
default:
break;
}
}
//****************************************************************************
//
//! callback event in case of MQTT disconnection
//!
//! \param app_hndl is the handle for the disconnected connection
//!
//! return none
//
//****************************************************************************
static void
sl_MqttDisconnect(void *app_hndl)
{
connect_config *local_con_conf;
event_msg msg;
local_con_conf = app_hndl;
msg.hndl = app_hndl;
msg.event = BROKER_DISCONNECTION;
UART_PRINT("disconnect from broker %s\r\n",
(local_con_conf->broker_config).server_info.server_addr);
local_con_conf->is_connected = false;
//
// write message indicating publish message
//
osi_MsgQWrite(&g_PBQueue,&msg,OSI_NO_WAIT);
}
//****************************************************************************
//
//! Push Button Handler1(GPIOS2). Press push button2 (GPIOSW2) Whenever user
//! wants to publish a message. Write message into message queue signaling the
//! event publish messages
//!
//! \param none
//!
//! return none
//
//****************************************************************************
void pushButtonInterruptHandler2()
{
event_msg msg;
msg.event = PUSH_BUTTON_SW2_PRESSED;
msg.hndl = NULL;
//
// write message indicating publish message
//
osi_MsgQWrite(&g_PBQueue,&msg,OSI_NO_WAIT);
}
//****************************************************************************
//
//! Push Button Handler3(GPIOS3). Press push button3 (GPIOSW3) Whenever user
//! wants to publish a message. Write message into message queue signaling the
//! event publish messages
//!
//! \param none
//!
//! return none
//
//****************************************************************************
void pushButtonInterruptHandler3()
{
event_msg msg;
msg.event = PUSH_BUTTON_SW3_PRESSED;
msg.hndl = NULL;
//
// write message indicating exit from sending loop
//
osi_MsgQWrite(&g_PBQueue,&msg,OSI_NO_WAIT);
}
//****************************************************************************
//
//! Toggles the state of GPIOs(LEDs)
//!
//! \param LedNum is the enumeration for the GPIO to be toggled
//!
//! \return none
//
//****************************************************************************
void ToggleLedState(ledEnum LedNum)
{
unsigned char ledstate = 0;
switch(LedNum)
{
case LED1:
ledstate = GPIO_IF_LedStatus(MCU_RED_LED_GPIO);
if(!ledstate)
{
GPIO_IF_LedOn(MCU_RED_LED_GPIO);
}
else
{
GPIO_IF_LedOff(MCU_RED_LED_GPIO);
}
break;
case LED2:
ledstate = GPIO_IF_LedStatus(MCU_ORANGE_LED_GPIO);
if(!ledstate)
{
GPIO_IF_LedOn(MCU_ORANGE_LED_GPIO);
}
else
{
GPIO_IF_LedOff(MCU_ORANGE_LED_GPIO);
}
break;
case LED3:
ledstate = GPIO_IF_LedStatus(MCU_GREEN_LED_GPIO);
if(!ledstate)
{
GPIO_IF_LedOn(MCU_GREEN_LED_GPIO);
}
else
{
GPIO_IF_LedOff(MCU_GREEN_LED_GPIO);
}
break;
default:
break;
}
}
//*****************************************************************************
//
//! Periodic Timer Interrupt Handler
//!
//! \param None
//!
//! \return None
//
//*****************************************************************************
void
TimerPeriodicIntHandler(void)
{
unsigned long ulInts;
//
// Clear all pending interrupts from the timer we are
// currently using.
//
ulInts = MAP_TimerIntStatus(TIMERA0_BASE, true);
MAP_TimerIntClear(TIMERA0_BASE, ulInts);
//
// Increment our interrupt counter.
//
g_usTimerInts++;
if(!(g_usTimerInts & 0x1))
{
//
// Off Led
//
GPIO_IF_LedOff(MCU_RED_LED_GPIO);
}
else
{
//
// On Led
//
GPIO_IF_LedOn(MCU_RED_LED_GPIO);
}
}
//****************************************************************************
//
//! Function to configure and start timer to blink the LED while device is
//! trying to connect to an AP
//!
//! \param none
//!
//! return none
//
//****************************************************************************
void LedTimerConfigNStart()
{
//
// Configure Timer for blinking the LED for IP acquisition
//
Timer_IF_Init(PRCM_TIMERA0,TIMERA0_BASE,TIMER_CFG_PERIODIC,TIMER_A,0);
Timer_IF_IntSetup(TIMERA0_BASE,TIMER_A,TimerPeriodicIntHandler);
Timer_IF_Start(TIMERA0_BASE,TIMER_A,100);
}
//****************************************************************************
//
//! Disable the LED blinking Timer as Device is connected to AP
//!
//! \param none
//!
//! return none
//
//****************************************************************************
void LedTimerDeinitStop()
{
//
// Disable the LED blinking Timer as Device is connected to AP
//
Timer_IF_Stop(TIMERA0_BASE,TIMER_A);
Timer_IF_DeInit(TIMERA0_BASE,TIMER_A);
}
//*****************************************************************************
//
//! Board Initialization & Configuration
//!
//! \param None
//!
//! \return None
//
//*****************************************************************************
void BoardInit(void)
{
/* In case of TI-RTOS vector table is initialize by OS itself */
#ifndef USE_TIRTOS
//
// Set vector table base
//
#if defined(ccs)
IntVTableBaseSet((unsigned long)&g_pfnVectors[0]);
#endif
#if defined(ewarm)
IntVTableBaseSet((unsigned long)&__vector_table);
#endif
#endif
//
// Enable Processor
//
MAP_IntMasterEnable();
MAP_IntEnable(FAULT_SYSTICK);
PRCMCC3200MCUInit();
}
//*****************************************************************************
//
//! Application startup display on UART
//!
//! \param none
//!
//! \return none
//!
//*****************************************************************************
static void
DisplayBanner(char * AppName)
{
UART_PRINT("\n\n\n\r");
UART_PRINT("\t\t *************************************************\n\r");
UART_PRINT("\t\t CC3200 %s Application \n\r", AppName);
UART_PRINT("\t\t *************************************************\n\r");
UART_PRINT("\n\n\n\r");
}
extern volatile unsigned long g_ulStatus;
//*****************************************************************************
//
//! Task implementing MQTT client communication to other web client through
//! a broker
//!
//! \param none
//!
//! This function
//! 1. Initializes network driver and connects to the default AP
//! 2. Initializes the mqtt library and set up MQTT connection configurations
//! 3. set up the button events and their callbacks(for publishing)
//! 4. handles the callback signals
//!
//! \return None
//!
//*****************************************************************************
void MqttClient(void *pvParameters)
{
long lRetVal = -1;
int iCount = 0;
int iNumBroker = 0;
int iConnBroker = 0;
event_msg RecvQue;
unsigned char policyVal;
connect_config *local_con_conf = (connect_config *)app_hndl;
//
// Configure LED
//
GPIO_IF_LedConfigure(LED1|LED2|LED3);
GPIO_IF_LedOff(MCU_RED_LED_GPIO);
GPIO_IF_LedOff(MCU_GREEN_LED_GPIO);
//
// Reset The state of the machine
//
Network_IF_ResetMCUStateMachine();
//
// Start the driver
//
lRetVal = Network_IF_InitDriver(ROLE_STA);
if(lRetVal < 0)
{
UART_PRINT("Failed to start SimpleLink Device\n\r",lRetVal);
LOOP_FOREVER();
}
// switch on Green LED to indicate Simplelink is properly up
GPIO_IF_LedOn(MCU_ON_IND);
// Start Timer to blink Red LED till AP connection
LedTimerConfigNStart();
// Initialize AP security params
SecurityParams.Key = (signed char *)SECURITY_KEY;
SecurityParams.KeyLen = strlen(SECURITY_KEY);
SecurityParams.Type = SECURITY_TYPE;
//
// Connect to the Access Point
//
lRetVal = Network_IF_ConnectAP(SSID_NAME, SecurityParams);
if(lRetVal < 0)
{
UART_PRINT("Connection to an AP failed\n\r");
LOOP_FOREVER();
}
lRetVal = sl_WlanProfileAdd(SSID_NAME,strlen(SSID_NAME),0,&SecurityParams,0,1,0);
//set AUTO policy
lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION,
SL_CONNECTION_POLICY(1,0,0,0,0),
&policyVal, 1 /*PolicyValLen*/);
//
// Disable the LED blinking Timer as Device is connected to AP
//
LedTimerDeinitStop();
//
// Switch ON RED LED to indicate that Device acquired an IP
//
GPIO_IF_LedOn(MCU_IP_ALLOC_IND);
UtilsDelay(20000000);
GPIO_IF_LedOff(MCU_RED_LED_GPIO);
GPIO_IF_LedOff(MCU_ORANGE_LED_GPIO);
GPIO_IF_LedOff(MCU_GREEN_LED_GPIO);
//
// Register Push Button Handlers
//
Button_IF_Init(pushButtonInterruptHandler2,pushButtonInterruptHandler3);
//
// Initialze MQTT client lib
//
lRetVal = sl_ExtLib_MqttClientInit(&Mqtt_Client);
if(lRetVal != 0)
{
// lib initialization failed
UART_PRINT("MQTT Client lib initialization failed\n\r");
LOOP_FOREVER();
}
/******************* connection to the broker ***************************/
iNumBroker = sizeof(usr_connect_config)/sizeof(connect_config);
if(iNumBroker > MAX_BROKER_CONN)
{
UART_PRINT("Num of brokers are more then max num of brokers\n\r");
LOOP_FOREVER();
}
connect_to_broker:
while(iCount < iNumBroker)
{
//create client context
local_con_conf[iCount].clt_ctx =
sl_ExtLib_MqttClientCtxCreate(&local_con_conf[iCount].broker_config,
&local_con_conf[iCount].CallBAcks,
&(local_con_conf[iCount]));
//
// Set Client ID
//
sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx,
SL_MQTT_PARAM_CLIENT_ID,
local_con_conf[iCount].client_id,
strlen((char*)(local_con_conf[iCount].client_id)));
//
// Set will Params
//
if(local_con_conf[iCount].will_params.will_topic != NULL)
{
sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx,
SL_MQTT_PARAM_WILL_PARAM,
&(local_con_conf[iCount].will_params),
sizeof(SlMqttWill_t));
}
//
// setting username and password
//
if(local_con_conf[iCount].usr_name != NULL)
{
sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx,
SL_MQTT_PARAM_USER_NAME,
local_con_conf[iCount].usr_name,
strlen((char*)local_con_conf[iCount].usr_name));
if(local_con_conf[iCount].usr_pwd != NULL)
{
sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx,
SL_MQTT_PARAM_PASS_WORD,
local_con_conf[iCount].usr_pwd,
strlen((char*)local_con_conf[iCount].usr_pwd));
}
}
//
// connectin to the broker
//
if((sl_ExtLib_MqttClientConnect((void*)local_con_conf[iCount].clt_ctx,
local_con_conf[iCount].is_clean,
local_con_conf[iCount].keep_alive_time) & 0xFF) != 0)
{
UART_PRINT("\n\rBroker connect fail for conn no. %d \n\r",iCount+1);
//delete the context for this connection
sl_ExtLib_MqttClientCtxDelete(local_con_conf[iCount].clt_ctx);
break;
}
else
{
UART_PRINT("\n\rSuccess: conn to Broker no. %d\n\r ", iCount+1);
local_con_conf[iCount].is_connected = true;
iConnBroker++;
}
//
// Subscribe to topics
//
if(sl_ExtLib_MqttClientSub((void*)local_con_conf[iCount].clt_ctx,
local_con_conf[iCount].topic,
local_con_conf[iCount].qos, TOPIC_COUNT) < 0)
{
UART_PRINT("\n\r Subscription Error for conn no. %d\n\r", iCount+1);
UART_PRINT("Disconnecting from the broker\r\n");
sl_ExtLib_MqttClientDisconnect(local_con_conf[iCount].clt_ctx);
local_con_conf[iCount].is_connected = false;
//delete the context for this connection
sl_ExtLib_MqttClientCtxDelete(local_con_conf[iCount].clt_ctx);
iConnBroker--;
break;
}
else
{
int iSub;
UART_PRINT("Client subscribed on following topics:\n\r");
for(iSub = 0; iSub < local_con_conf[iCount].num_topics; iSub++)
{
UART_PRINT("%s\n\r", local_con_conf[iCount].topic[iSub]);
}
}
iCount++;
}
if(iConnBroker < 1)
{
//
// no succesful connection to broker
//
goto end;
}
iCount = 0;
for(;;)
{
char buffer1[]=UartGetChar1();
// buffer12[i] = buffer1[0];
// i++;
char *data_sw3= buffer1;
sl_ExtLib_MqttClientSend((void*)local_con_conf[iCount].clt_ctx,
pub_topic_sw3,data_sw3,strlen((char*)data_sw3),QOS0,RETAIN);
// osi_MsgQRead( &g_PBQueue, &RecvQue, OSI_WAIT_FOREVER);
if(PUSH_BUTTON_SW2_PRESSED == RecvQue.event)
{
Button_IF_EnableInterrupt(SW2);
//
// send publish message
//
sl_ExtLib_MqttClientSend((void*)local_con_conf[iCount].clt_ctx,
pub_topic_sw2,data_sw2,strlen((char*)data_sw2),QOS0,RETAIN);
UART_PRINT("\n\r CC3200 Publishes the following message \n\r");
UART_PRINT("Topic: %s\n\r",pub_topic_sw2);
UART_PRINT("Data: %s\n\r",data_sw2);
}
// else if(PUSH_BUTTON_SW3_PRESSED == RecvQue.event)
// {
// Button_IF_EnableInterrupt(SW3);
//
// send publish message
//
// UART_PRINT("\n\r CC3200 Publishes the following message \n\r");
// UART_PRINT("Topic: %s\n\r",pub_topic_sw3);
// UART_PRINT("Data: %s\n\r",data_sw3);
// }
else if(BROKER_DISCONNECTION == RecvQue.event)
{
iConnBroker--;
/* Derive the value of the local_con_conf or clt_ctx from the message */
sl_ExtLib_MqttClientCtxDelete(((connect_config*)(RecvQue.hndl))->clt_ctx);
if(!IS_CONNECTED(g_ulStatus))
{
UART_PRINT("device has disconnected from AP \n\r");
UART_PRINT("retry connection to the AP\n\r");
while(!(IS_CONNECTED(g_ulStatus)) || !(IS_IP_ACQUIRED(g_ulStatus)))
{
osi_Sleep(10);
}
goto connect_to_broker;
}
if(iConnBroker < 1)
{
//
// device not connected to any broker
//
goto end;
}
}
}
end:
//
// Deinitializating the client library
//
sl_ExtLib_MqttClientExit();
UART_PRINT("\n\r Exiting the Application\n\r");
LOOP_FOREVER();
}
//*****************************************************************************
//
//! Main
//!
//! \param none
//!
//! This function
//! 1. Invokes the SLHost task
//! 2. Invokes the MqttClient
//!
//! \return None
//!
//*****************************************************************************
void main()
{
long lRetVal = -1;
//
// Initialize the board configurations
//
BoardInit();
//
// Pinmux for UART
//
PinMuxConfig();
//
// Configuring UART
//
InitTerm();
//
// Display Application Banner
//
DisplayBanner("MQTT_Client");
//
// Start the SimpleLink Host
//
lRetVal = VStartSimpleLinkSpawnTask(SPAWN_TASK_PRIORITY);
if(lRetVal < 0)
{
ERR_PRINT(lRetVal);
LOOP_FOREVER();
}
//
// Start the MQTT Client task
//
osi_MsgQCreate(&g_PBQueue,"PBQueue",sizeof(event_msg),10);
lRetVal = osi_TaskCreate(MqttClient,
(const signed char *)"Mqtt Client App",
OSI_STACK_SIZE, NULL, 2, NULL );
if(lRetVal < 0)
{
ERR_PRINT(lRetVal);
LOOP_FOREVER();
}
//
// Start the task scheduler
//
osi_start();
}
Note- When I sent characters value from Transmitter side i.e char buffer[6]= "ABC"; It get received to server .
Main issue to not getting hex values .Please help to overcome this issue.
Thanks & Regards,
Shashank